Part Number: TMS320F28388D
Dear,
Regarding the 28388D program with CPU1, CPU2, CLA1, CLA2, and CM equivalent to 5 cores, may I ask about the issue of program burning:
1. Is it necessary to first use JTAG to burn the program before using other programs such as SCI or CAN? Is there a way for a brand new chip to burn programs through an external communication interface even when powered on for the first time?
2. Can all five cores mentioned above be upgraded through non JTAG ports?
3. Due to the large number of devices on site, there may be tens of thousands of devices on one site. Therefore, we hope to improve the efficiency of program upgrades. Can we use a network port to write programs? If it doesn't work, are there any other options?