Hi to all ,
I’m working on a system very close to the HVMotorCtrl+PfcKit_v1.6 , with an F28035 , a different power module and a hw current limit protection at about 25amps .
My target is to drive a HVPM brushless motor 8 pole at 10’000 rpm , in sensorless mode , that means about 670 Hz .
Isr and PWM are 20KHZ , as in the kit .
The system can measure up to 20amps , but I set the Out max at 0.8 , that means 16amps .
The dc bus is 310Vdc , with higher current that needed .
With this set-up , I can’t go over 7’000 rpm . What I see is a high current ( more than 20amps ) on the motor phases , while current regulator (pid1_iq.out) Is less the 0.5 ( 10amps).
I think speed and current regulator are tuned correctly , I think also I’ve something to tune in the SMO .
In fact I tried to change some parameters in the SMO , obtaining lower current in the phases and higher speed in the motor , but there are higher difference from requested current and measured current , so hw current limiter sometimes happens .
I made some tests with this motor , in the same application , using a commercial FOC frequency converter , and I’m sure less the 10 amps are required , I measured about 5amps at rated speed and 8 amps during the ramp-up.
Can you suggest something to do ?
Thanks
Andreas