Part Number: TIDM-1000
Other Parts Discussed in Thread: SFRA
Hi Team,
Greetings of the day!
We are using TIDM-1000 Software for our custom board with our ADC scale factor and Passive element parameters.
Now we want to change compensation designer type from One Pole one Zero to 2 Poles 2 Zeros. Here we will get the output parameters(B0,B1,B2,A1,A2) for 2-pole 2-zero differently.
How those parameters will be given to the code(in the form of Kp and Ki or anything else)?
There are many coefficient's in "Kit.json" file as shown in the below, but Now our question is where we have to give the input of compensation coefficients(A0,A1,A2,B1,B2) after tuning(poles and zeros frequencies) which we got from the GUI (SFRA Analyzer tool).
{
"MODEL": {
"ID": "4",
"PLANT": {
"Fsw": "50000",
"Fctrl": "50000",
"Tuning": "2",
"Vin": "208",
"Vout": "600",
"Pout": "680",
"Vout_SenseMax": "454",
"I_SenseMax": "12",
"Li": "0.003",
"Ri": "0.2",
"Cf": "0.00018",
"Rcf": "0.73",
"Rfltr": "68",
"Cfltr": "1.0000000000000001e-7",
"ProjectNonModifiable": "0"
},
"COMP": [
{
"TUNING": "9",
"DCL_Kp": "0.349650340737655",
"DCL_Ki": "0.00200005103159284",
"A0": "1",
"A1": "1",
"A2": "0",
"A3": "0",
"B0": "2",
"B1": "0",
"B2": "0",
"B3": "0",
"z0": "31831",
"Qz0": "4.68705446301803",
"z1": "13418",
"z2": "1000000",
"p0": "0",
"p1": "31831",
"Qp1": "1",
"p2": "20000000000000",
"gain": "60730.2403614083",
"Kp": "2",
"Ti": "0.00018896447",
"Td": "0"
},
{
"TUNING": "10",
"DCL_Kp": "0.1486725877128",
"DCL_Ki": "3.38095160854676",
"A0": "1",
"A1": "1",
"A2": "0",
"A3": "0",
"B0": "0.40004",
"B1": "-1.39996",
"B2": "0",
"B3": "0",
"z0": "10000",
"Qz0": "4.68705446301803",
"z1": "13418",
"z2": "1000000",
"p0": "0",
"p1": "31831",
"Qp1": "1",
"p2": "20000000000000",
"gain": "0.4",
"Kp": "0.4",
"Ti": "0.1",
"Td": "0"
},
{
"TUNING": "9",
"DCL_Kp": "0.349650340737655",
"DCL_Ki": "0.00200005103159284",
"A0": "1",
"A1": "0",
"A2": "0",
"A3": "0",
"B0": "1",
"B1": "0",
"B2": "0",
"B3": "0",
"z0": "31831",
"Qz0": "4.68705446301803",
"z1": "13418",
"z2": "1000000",
"p0": "0",
"p1": "31831",
"Qp1": "1",
"p2": "20000000000000",
"gain": "91095.0964494984",
"Kp": "1",
"Ti": "1E-06",
"Td": "0"
}
],
"COMP_OPTIONS": {
"COMP_NUM": "2",
"MODEL_STYLE": "1",
"SFRAPATH": "C:/pfc3phvienna_F28004x/SFRAData/SFRAData.csv",
"COMP_ABS_LIMIT": "256",
"COMP_STYLE": "10"
}
}
}
Thank you in Advance!
Regards,
Chaithanya.