Other Parts Discussed in Thread: C2000WARE
I want to run led example code in my LAUNCHXL-F2800157 board,but LED4/LED5 was not blink.Here are some of my configurations.




This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to run led example code in my LAUNCHXL-F2800157 board,but LED4/LED5 was not blink.Here are some of my configurations.




Hi,
Currently we have moved the LED blinky example to universal format in C2000Ware SDK 5.02.
This is basically helpful to migrate between devices.
So if you need to load the example in Launchpad, please make the following changes -
1) Update the build configuration to CPU1_Launchxl_RAM
2)Open the syscfg file -> click on board option -> show device view -> switch option -> choose device as launchpad_f2800157
This should make the necessary launchpad configuration required.
If you are using older version of C2000Ware SDK, please download the latest SDK V5.02 from ti.com.
Thanks
Aswin