This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Programming TMS320F2837D from bananapi-m64 via xds110/xds100v3

Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH

Hi,

For producton purpose I need to program TMS320F2837D via xds110 or xds100v3 (flash and otp memories).

This works fine when laptop is the host and I use UniFlash software. 

I need to do the same but from bananapi-m64 (arm with linux arch=aarch64) without display - only console access.

I assume that I would need some build of the uniflash command line version for that cpu architecture [?]. 

Can you give me any directions how to start with that? 

Regards,
Piotr Romaniuk