Part Number: LAUNCHXL-F28027F
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Can anyone help me out. I installed CCS IDE 12.7.0.00007 and also Installed controlSUITE3.4.9setup. when I import GPIO Toggle from this path (C:\ti\controlSUITE\device_support\f2802x\v230\f2802x_examples_structs), Am facing an Error i.e.,
Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed - 6.4.2 [C2000]. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="">software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. Example_2802xGpioToggle properties Problem.
----> I tried out by going into 'Help' window and Installed New Software->'Code Generation Tools Updates'. But there is no version with 6.4.2[C2000]. In TI site, I serached all CCS versions release notes in TI site,but there is no CCS IDE which is having 6.4.2[C2000] compiler Version compatibility.
----> Hope someone will help me out to how to resolve this Issue and to run the Example projects and as well as my custom applications.
regards,
Tarun.