Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH
Hi,
I would like to program TMS320F28379D (flash and otp memory) from linux command line.
I am struggling with Uniflash under linux. I have Intel Atom 330 board which is x86_64.
So far I tested:
- xubuntu 16.04 - Uniflash can be installed and run, but is not detecting xds110. In syslog there is some complains about glibc version (too old)
- ubuntu 20.04.6 LTS - Cannot install Uniflash, installer display message that libusb and libgconf are missing (unfortunatelly these libraries are no longer in the distribution)
I was informed that UniFlash is supported for Linux and x86-64 architecture.
Please tell me what Linux (distribution and version) should I use to have UniFlash working.
This is very critical for me, in one week programming of 1k devices with TMS320F28379D must be started.
UniFlash is only a component for me, I need to build the environment that is based on UniFlash.
Regards,
Piotr Romaniuk