Part Number: TMS320F28075
Other Parts Discussed in Thread: SYSCONFIG, SFRA, C2000WARE
Hi Omer,
We are having issues migrating from 280049 to 2837x and 2807x families within Code Composer Studio.
Context: Manish from TI helped us debug the original Bridgeless TTPFC Project with the 280049 device. We have been successful in bringing the project through all of its phases, up to Full Power. Now we are looking to migrate from 280049 to either the 37x or 07x family.
You have been very helpful in providing us with the link to access the SysConfig tool; however we have been receiving several CLA errors when attempting to migrate from 049 to 37x and 07x (please see attached images with corresponding errors: Exhibit 4).
Due to these CLA errors, the build fails to update the "Generated Files" to the target processor.
Also, the generated files don't seem to include the pin mapping file from the source (049) to the target.
Additionally, we are not able to locate the 075 or 377s devices when using the "Switch" feature. Instead, we used 076 and 378s as targets, as only these were available as switch options.
Could you please advise us on how we can resolve these errors?
Thanks!