Part Number: TMS320F280036C-Q1
What I want is to flash boot, but I also want to use HIC_D3. The chip I am using is 280036C.
The manual states that to use flash boot, gpio24 and gpio 32 must be pulled up.
The first question is: Can I use GPIO24 pin as HIC_D3 while using it as BOOT pin?
The second question is
If the above situation is possible, the BOOT PIN must be pulled up. Does it work normally even if HIC_D3 is pulled up?
thank you