This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000-GANG: For TMS320F28375D.

Part Number: C2000-GANG
Other Parts Discussed in Thread: UNIFLASH

Dear Sir / Madam

We are using your C2000-GANG programmer in a manufacturing system to program the referenced MCU.

We need to programme a panel of four identical PCBAs and have problems with one of the boards within the panel.

This is persistent across several panels therefore we consider this could be cause by a difference in the hardware, nevertheless do not discard any other issue with the configuration of the firmware.

as the connections for the four pcbas are identical and we have discarded the boards from being defective.

The JTAG connection is direct to the each of the individual boards, we have the included wires and 5cm of single wire to the nails.

R - C between the CLK and the GND  68ohm - 100pf as recommended

The error we get is ERROR 23: MCD device init

Please can you help us to fix this?

Thanks in advance