Part Number: TIDM-1000
Other Parts Discussed in Thread: SFRA
Dear Team,
We are facing two kind of issues, One is at no-load and 25W load condition the output voltage is not regulating (we need the output voltage to regulate at 380V instead it was generating 420V) and the second was, while introducing the load of 1000W suddenly from no-load the output voltage drops to 320 and starts to rise and gets stabled in 370 instead of 380V, so to solve this problems we change the "VIENNA_GV_PI_MIN" Value from -0.02 to -0.1, Which have solve our problem for 25W load but making the second problem even worse(when introduce the sudden load of 1000W the output voltage drops to 320V and stables at 340V
So can you please suggest something regards this problems and how this Kp, Ki gain MIN and MAX values were calculated, How these values are going to affect the systems output.