Part Number: TMS320F28379D
Hi
I am using ADCA as differential mode and ADCB as single ended and triggering all ADC channel with EPWM5 , I am able to receive the data from the channel that are written in ADC A ISR but unable to get into ADC B ISR.
Attaching the code below .
I really appreciate it if you take a look and see which part of the code I need to change
Thanks in Advanced .
#include "F28x_Project.h"
#include "math.h"
//float32 PI 3.14159265359;
extern void InitSysCtrl(void);
void Gpio_select(void);
void Setup_ePWM(void);
void ConfigureADC(void);
void SetupADCSoftware(void);
interrupt void adcAINT1_isr(void);
interrupt void adcBINT2_isr(void);
//variables
float32 PI= 3.14159265359;
float32 AdcaResult_Current=0;
float32 AdcaResult_Current1=0;
float32 sub_current=0;
float32 AC_input_vtg =0;
float32 AC_input_current =0;
float32 DC_output_vtg = 0;
float32 Actual_AC_input_vtg =0;
float32 Actual_AC_input_current =0;
float32 Actual_DC_output_vtg = 0;
Uint32 EPwm_time_counter= 0 ;
//variable used for implementing Low pass filter for offset cal
float32 Current_offset=0;
float32 Current_offset_Old=0;
float32 AdcaResult_Current_Old=0;
float32 f1 = 10; // low pass filter cutoff frequency
float32 Tsw = 0.000008;
//variable for stopping the loop of 10 sec and ON the EPWM for one time
int initialize=5;
//*********Protection for PFC converter*********//
float32 Actual_Current_result=0;
float32 Current_Limit_Positive=10;
float32 Current_Limit_Negative=-10;
float32 DC_link_Limit_Positive=100;
float32 DC_link_Limit_Negative=-1;
int inc=0;
Uint32 cheque_counter=0;
int m=0; // check if code line passes to main Closed loop code
int TBPRD =800;
// variable for Ramp Input Current to Boost Converter
int Normal_Operation_Counter=0;
Uint32 Soft_Start_Counter=0;
float32 Current_inc=0;
//Current PI variable
int Duty_count=0;
float32 Current_Ref = 5; //RMS
float32 Ref_Current_1 = 0;
float32 Error_Current_new_1=0;
float32 Actual_Current_1=0; //Actual Current
float32 Duty_new_1=0;
float32 K1_i=0.01012985999999999747744894;
float32 K2_i=0.009034739999999999437996223;
float32 Error_Current_old_1=0;
float32 Duty_old_1=0;
//Digital Low Pass Filter
float32 sub_current_new=0;
float32 sub_current_new_filter=0;
float32 sub_current_old_filter=0;
float32 sub_current_old=0;
void main(void)
{
InitSysCtrl();
DINT;
Gpio_select();
Setup_ePWM();
EALLOW;
ClkCfgRegs.PERCLKDIVSEL.bit.EPWMCLKDIV = 0;
ConfigureADC();
SetupADCSoftware();
EDIS;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW;
PieVectTable.ADCA1_INT=&adcAINT1_isr;
PieVectTable.ADCB1_INT=&adcBINT2_isr;
IER |= M_INT1;
IER |= M_INT2;
PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
PieCtrlRegs.PIEIER1.bit.INTx2 = 1;
EINT;
ERTM;
EDIS;
while(1)
{
}
}
void Gpio_select(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO8=1; // ePWM5A active used to take sample
GpioCtrlRegs.GPAMUX1.bit.GPIO9=0; // Setting pin as GPIO Relay
GpioCtrlRegs.GPADIR.bit.GPIO9=1; //setting pin as output pin
GpioCtrlRegs.GPAMUX1.bit.GPIO10=1; // ePWM6A active for fast leg top
GpioCtrlRegs.GPAMUX1.bit.GPIO11=1; // ePWM6B active for fast leg bottom
GpioCtrlRegs.GPAMUX1.bit.GPIO4=0; //Setting pin as gpio slow leg top
GpioCtrlRegs.GPADIR.bit.GPIO4=1; //setting pin as output pin
GpioCtrlRegs.GPAMUX1.bit.GPIO5=0; //Setting pin as gpio slow leg bottom
GpioCtrlRegs.GPADIR.bit.GPIO5=1; //setting pin as output pin
GpioCtrlRegs.GPBMUX1.bit.GPIO32=0; //Setting pin as gpio check
GpioCtrlRegs.GPBDIR.bit.GPIO32=1; //setting pin as output pin
EDIS;
}
void ConfigureADC(void)
{
EALLOW;
AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //Divide by 4 so 200MHz/4=50Mhz
AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_DIFFERENTIAL);
AdcSetMode(ADC_ADCB, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;//power up ADC
EDIS;
DELAY_US(1000);
}
void SetupADCSoftware(void)
{
Uint16 acqps; // acquisition time
if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION)
{
acqps = 14; //75ns
}
else
{
acqps =63;//320ns
}
EALLOW;
AdcaRegs.ADCSOC0CTL.bit.CHSEL = 0; //AC current 1
AdcaRegs.ADCSOC0CTL.bit.ACQPS = acqps;
AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 13;//here we are specifically telling that epwm5A is start of conversion for ADCA2
AdcaRegs.ADCSOC1CTL.bit.CHSEL = 1; // AC current 2
AdcaRegs.ADCSOC1CTL.bit.ACQPS = acqps;
AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = 13;//here we are specifically telling that epwm5A is start of conversion for ADCA2
AdcbRegs.ADCSOC2CTL.bit.CHSEL = 2; // AC Grid Voltage
AdcbRegs.ADCSOC2CTL.bit.ACQPS = acqps;
AdcbRegs.ADCSOC2CTL.bit.TRIGSEL = 13;//here we are specifically telling that epwm5A is start of conversion for ADCA2
AdcbRegs.ADCSOC3CTL.bit.CHSEL = 3; // DC link Voltage
AdcbRegs.ADCSOC3CTL.bit.ACQPS = acqps;
AdcbRegs.ADCSOC3CTL.bit.TRIGSEL = 13;//here we are specifically telling that epwm5A is start of conversion for ADCA2
AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1(ADCA_ISR1) flag
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared
AdcbRegs.ADCINTSEL1N2.bit.INT2SEL = 3; //end of SOC3 will set INT2(ADCB_ISR2) flag
AdcbRegs.ADCINTSEL1N2.bit.INT2E = 1; //enable INT2 flag
AdcbRegs.ADCINTFLGCLR.bit.ADCINT2 = 1; //make sure INT2 flag is cleared
EDIS;
}
void Setup_ePWM(void)
{
//EPWM 5A for controlling ADC sampling
EPwm5Regs.TBCTL.bit.CLKDIV=0; //(Set clock division=00) divide by 1
EPwm5Regs.TBCTL.bit.HSPCLKDIV=0; //(Set high speed clock division=00)divide by 1
EPwm5Regs.TBCTL.bit.CTRMODE=2; //up-Down Mode
EPwm5Regs.TBPRD=TBPRD; //Period corresponding to 125kHz
EPwm5Regs.CMPA.bit.CMPA =TBPRD*0.5; //50% duty cycle
EPwm5Regs.AQCTLA.all=0x0090; //set high when TBCTR=CMPA and low when TBCTR=0
EPwm5Regs.TBCTL.bit.SYNCOSEL=TB_CTR_ZERO; //Giving a SYS out bit at TBCTL zero
EPwm5Regs.TBPHS.bit.TBPHS=0; //Set phase angle of ePWM4 is 0
EPwm5Regs.TBCTL.bit.PHSEN=0; //Set as a master
EPwm5Regs.TBCTL.bit.PRDLD = TB_SHADOW; //The period register (TBPRD) is loaded from its shadow register
EPwm5Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; //Shadow mode
EPwm5Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; //Load on CTR = Zero: Time-base counter equal to zero
EPwm5Regs.ETSEL.bit.SOCAEN = 1; //Epwm5A is used as start of conversion for ADC
EPwm5Regs.ETSEL.bit.SOCASEL = 1; //Enable event time based counter to zero
EPwm5Regs.ETPS.bit.SOCAPRD = 3; //at every third event it has to generate event
EPwm5Regs.ETCLR.bit.SOCA = 1; //Clear flag
EPwm5Regs.ETSEL.bit.INTEN = 0; //Enable ePWM Interrupt (EPWMx_INT) Generation
EPwm5Regs.ETSEL.bit.INTSEL = 1; //enable event time
EPwm5Regs.ETPS.bit.INTPRD = 3; //at every third event it has to generate event
EPwm5Regs.ETCLR.bit.INT = 1; //Clear flag
//EPWM 6 for controlling 125KHz legs
EPwm6Regs.TBCTL.bit.CLKDIV=0; //(Set clock division=00) divide by 1
EPwm6Regs.TBCTL.bit.HSPCLKDIV=0; //(Set high speed clock division=00)divide by 1
EPwm6Regs.TBCTL.bit.CTRMODE=2; //up-Down Mode
EPwm6Regs.TBPRD=TBPRD; //Period corresponding to 125kHz
EPwm6Regs.CMPA.bit.CMPA =TBPRD*0.5; //38% duty cycle
EPwm6Regs.DBCTL.bit.POLSEL = 2; //Active High Complementary inverted signal will be observed at ePWMB
EPwm6Regs.DBCTL.bit.OUT_MODE = 3; //fully enabled RED and FED
EPwm6Regs.DBRED.all = 0; //RED 200ns
EPwm6Regs.DBFED.all = 0; //FED 200ns
EPwm6Regs.AQCTLA.all=0x0090; //set high when TBCTR=CMPA and low when TBCTR=0
EPwm6Regs.TBCTL.bit.SYNCOSEL=0; //Giving a SYS in bit
EPwm6Regs.TBCTL.bit.PHSDIR=1;
EPwm6Regs.TBCTL.bit.PHSEN=1; //Set as a slave
EPwm6Regs.TBPHS.bit.TBPHS=2; //Set phase angle of ePWM2 is 0
}
interrupt void adcAINT1_isr(void)
{
AdcaResult_Current = AdcaResultRegs.ADCRESULT0; //AdcaResult_Current and AdcaResult_Current1 both values are almost same
AdcaResult_Current1 = AdcaResultRegs.ADCRESULT1;
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
if(1 == AdcaRegs.ADCINTOVF.bit.ADCINT1)
{
AdcaRegs.ADCINTOVFCLR.bit.ADCINT1 = 1; //clear INT1 overflow flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
}
PieCtrlRegs.PIEACK.bit.ACK1 = PIEACK_GROUP1;
}
interrupt void adcBINT2_isr(void)
{
m=1;
GpioDataRegs.GPBSET.bit.GPIO32=1;
AC_input_vtg = AdcbResultRegs.ADCRESULT2;
// AC_input_current = AdcaResultRegs.ADCRESULT1 - AdcaResultRegs.ADCRESULT2; //AdcaResult_Current and AdcaResult_Current1 both values are almost same
DC_output_vtg = AdcbResultRegs.ADCRESULT3;
AdcbRegs.ADCINTFLGCLR.bit.ADCINT2 = 1;
if(1 == AdcaRegs.ADCINTOVF.bit.ADCINT2)
{
AdcaRegs.ADCINTOVFCLR.bit.ADCINT2 = 1; //clear INT1 overflow flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT2 = 1; //clear INT1 flag
}
PieCtrlRegs.PIEACK.bit.ACK2 = PIEACK_GROUP1;
GpioDataRegs.GPBCLEAR.bit.GPIO32=1;
//reset
}