Other Parts Discussed in Thread: TMDSHSECDOCK, C2000WARE, SYSCONFIG
Hello there!
I am totally new to MCU programming. Trying to program the board (f28p65x) as as Master SPI Controller. I can load and run some examples provided in the SDK.
My question is, how to map or assign SPI signals (SPIPICOA, SPIPOCIA, SPICLKA, SPIPTEA) to the Docking station (TMDSHSECDOCK), so a slave SPI device can be connected and controlled by MCU?
Connecting slave device to pins 67, 69, 71, 73, does not output any signals.
Please any suggestion, any steps I am missing or have to be done to make outputs active?
Are there any particular examples that do that exact function of controlling slave SPI device via (f28p65x) MCU board?
Thanks,
Sergey.