Other Parts Discussed in Thread: C2000WARE
Hi,
I am trying to share a ccs project to one more colleague. This is executed properly when executed in my system. But in their system it is resulting in compilation errors. The error message is as follows:
**** Build of configuration Debug for project 001_PHASE_C **** "C:\\ti\\ccs1260\\ccs\\utils\\bin\\gmake" -k -j 8 all -O Building file: "../application/main.c" Invoking: C2000 Compiler "C:/ti/ccs1260/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcrc --include_path="C:/CCS/Learning/001_PHASE_C" --include_path="C:/CCS/Learning/001_PHASE_C/drivers" --include_path="C:/CCS/Learning/001_PHASE_C/hal" --include_path="C:/ti/ccs1250/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/include" --include_path="C:/CCS/Learning/001_PHASE_C/Debug/syscfg" --advice:performance=all -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=coffabi --preproc_with_compile --preproc_dependency="application/main.d_raw" --include_path="C:/Users/10861368/commTI/001_PHASE_C_V5/001_PHASE_C_V5/001_PHASE_C/Debug/syscfg" --obj_directory="application" "../application/main.c" >> Compilation failure application/subdir_rules.mk:9: recipe for target 'application/main.obj' failed "../application/main.c", line 56: fatal error #1965: cannot open source file "stdlib.h" 1 catastrophic error detected in the compilation of "../application/main.c". Compilation terminated. gmake: *** [application/main.obj] Error 1 gmake: Target 'all' not remade because of errors. **** Build Finished ****
NOTE:
1) my includes in project properties