This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025C: TMS320F280025C

Part Number: TMS320F280025C

Iam using TMS320F280025C + DRV8343.

Inputs entered in coding is based on the motor parameters.

1.I want to increase the torque to 6 Nm.

what parameter should i tune to increase the torque?

  • Assuming you are using the lab based on InstaSPIN-FOC. Please take a look at the lab user's guide. You can increase the maximum current according to the motor. And also take a look at the datasheet of DRV8343 to increase its current limitation by setting its control registers. 

    // the maximum current value of the motor, in A
    #define USER_MOTOR1_MAX_CURRENT_A (9.5f)

  • 1.Generally, at input side current drawn with respect to load/torque variation, if it's more torque it drawn more current, in our cases motor drawn more current in input side but estimator window shows very less torque (E.g:- at the time of 22A motor delivers around 0.5Nm but estimator window shows 0.192Nm only).

    could you please clarify this.

  • You may check if the motor and hardware parameters are set correctly according to the system you are working on. The calculation torque is fully related to these parameters.