Part Number: LAUNCHXL-F280039C
Number: CS2328744
Contact: Aditi Patil
First name: Aditi
Last name: Patil
Short description: LAUNCHXL-F280039C: CLA subsytem
Email: aditi.patil@external.forvia.com
Company: Forvia Hella
Company phone:
Language: English
State: Work in progress
Provide case details or comments:
Hello I want to use CLA task subsytem for code generation for my project
So first I started from basic like LED blinking and for that in CLA subsytem I built a logic where pulse generator is connected to launchpad GPIO but when I started to build project its shows to inherit sample time to -1 and due to this my all setting will be in term of number of sample as it will be challenging in simulink
Provide me a solution
yes but as we know there are two modes for pulse generator time and sample based mode so i want in time mode because it will be easy for critical task . so as we have parameters like period,phase delay ,pulse width for time based and according to that i set period 2 sec pulse width 50% and phase delay 0 so after that I configured digital output GPIO to inbuild LED on launchpad F280039c which is 22 and build the model after that it shows error that inherit sample time of pulse generator t0 -1 so for that i want to change time mode to sample mode and all period,phase delay,pulse width they ask in number of samples which is challenging for me