Part Number: TMS320F28386S
Hi All,
I just booted the USB boot loader with emulation boot of F28386S,
The PC shows "unknown device" and not boot.
Currently I am using a 25MHz oscillator.
I saw an article on TI's forum that the USB bootloader only works with a 20MHz oscillator.
(+) TMS320F28388D: USB-Boot Loader isn't recognized by Windows, when using 25 MHz oscillator - C2000 microcontrollers forum - C2000︎ microcontrollers - TI E2E support forums
Is this still the case?
If so, is there any way around this?
Best Regards,
Ito