Part Number: TMS320F28035
Dear Expert
TMS320F28035 encountered the issue of CLA not running. Can it be supported!
After debugging the engineering burning and connecting the target to CLA, and downloading the RUN ->Load ->Load Symbols, the CPU runs at full speed and is displayed on the Debug page, as shown in the following figure:
At the same time, it is displayed on the Disambly interface, as shown in the following figure.


(The next page shows the detailed configuration code)
CLA initialization;

CLA interrupt

CLA trigger source