This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800156-Q1: Linker generated CRC does not match with computed CRC

Part Number: TMS320F2800156-Q1

Hi,

I have a custom booloder code. I want to check CRC of application code in bootloder. 

I created section for my application and CRC result in the linker file.

MEMORY
{
    GROUP(FLASH)
    {
        BEGIN   : origin = 0x090000, length = 0x00000002
        APPCODE : origin = 0x090002, length = 0xE000-0x80-0x02
    } crc(linkerCrcRecord, algorithm=CRC32_PRIME)
    
    CRC_TABLE   : origin = 0x09DF80, length = 0x000080
}

SECTIONS
{
    .TI.memcrc > CRC_TABLE
}

I am computing crc with this code in the bootloder.

    MEMRANGE_CRC_TABLE *pLinkerCrcTable;

    pLinkerCrcTable  = (MEMRANGE_CRC_TABLE*)(0x09DF80);

    uint32_t goldenCRC = pLinkerCrcTable->crc_value;
    
    CRC_Obj    CRC;
    // \brief handle(pointer) to the CRC object
    //
    CRC_Handle handleCRC;
    // \brief A single record(element) from the CRC table object

    // Step 2: Initialize the CRC object
    CRC.seedValue    = INIT_CRC32;
    CRC.nMsgBytes    = 0xDF80;
    CRC.parity       = CRC_parity_even;
    CRC.crcResult    = 0;
    CRC.pMsgBuffer   = (uint32_t*)(void*)(0x090000U);
    CRC.pCrcTable    = NULL;
    CRC.init         = (void (*)(void *))CRC_init32Bit;
    CRC.run          = (void (*)(void *))CRC_run32BitPoly1;

    // Step 3: Initialize the handle
    handleCRC = &CRC;

    // Step 2: Run the VCU 32-bit CRC routine and save the result
    CRC.run(handleCRC);

    // Compare calculated CRC and golden CRC.
    if(goldenCRC != CRC.crcResult)
    {
    //does not match
    }
    

Computed CRC and linker generated CRC does not match. 

Where am I doing wrong?