Part Number: TMS320F28035
Other Parts Discussed in Thread: C2000WARE
HI experts,
My customer has trouble using the f2803x's comparator for overvoltage protection. The trigger route is (comp2A vs DAC) -> DCBH -> DCBEVT1 -> one-shot latch.
When they use hysteresis, the TZ can be triggered at the correct voltage level. However, once it's triggered, the voltage at the comp input pin has a 200mV step-up.
When not using hysteresis, the TZ is triggered all the time. Clearing the one-shot flag has no effect. The COMPSTS is 0, but DCBEVT1 is still triggered (Same when inverting the COMPOUT polarity).
Is the voltage step-up normal? Way DCBEVT still triggers when COMPSTS is 0?
Regards,
Hang.