This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2809: MAX_CONV1=7 with CONT_RUN=0 using ADC dual sequencer mode

Part Number: TMS320F2809

Dear Champs,

I am asking this for our customer.

This is an extension project with an old design on F2809, and new FW guys are picking the old design and modifying a little bit.

For ADC, the user uses dual sequencer mode, 

CONT_RUN=0

MAX_CONV1=7

The user wonders if they don't reset sequencer in the end of ADC ISR below,

AdcRegs.ADCTRL2.bit.RST_SEQ1=1;

can SEQ1 wrap around to CONV00 again after SEQ1 ends at CONV7 and then gets triggered even with CONT_RUN=0?

They are asking this because they find it does not matter if they remove AdcRegs.ADCTRL2.bit.RST_SEQ1=1; in the end of ADC ISR.

Therefore, they want us to confirm this.