This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: f28388D

Part Number: TMS320F28388D


Hello,

While testing the watchdog on while flashing - (we use FlashAPI) the processor on board was blocked. I can't load new hex file to processor.

Please help me for a solution to the problem.

I added the logs from CCS below:

"Error connecting to the target: (Error -1135 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.

(Emulation package 9.8.0.00235)"

OR:

Error connecting to the target:

(Error -1015 @ 0x0)

"Device is not responding to the request.  Device may be locked, or the debug probe connection may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board). If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).

(Emulation package 9.3.0.00058)"