Hi,
I am using the Universal Motor Control Lab project to spin my motor. The speed control seems to work well until 0.1Hz (0.4rpm), but it still spins (in opposite direction) when I apply a speed ref of 0Hz.
I have tested with the FAST estimator and with my encoder (angle value without noise). I need that to be able to implement the position control.
Thank you in advance for your support,
David