This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800132: Cannot run TIDA-010265 in F2800132

Part Number: TMS320F2800132
Other Parts Discussed in Thread: TIDA-010265,

Hi Team

I try to download the project of TIDA-010265, but it report the issue: Break at address "0x3fff08" with no debug information available, or outside of program code.

Click View disassembly, it shows:

I try to make some changes in the existing project:

1. change the 120Mhz to 100Mhz -- do not work

2. change the device in .projectspec -- do not work

3. run the project step by step and block line 178 -- work.

 systemVars.estLibVersion = EST_getFASTVersion();   // gets FAST version

4. review the .map file for the function location, seems no issue here:

Thanks and best regards

Joe

16th May