This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Using CAN bitfield API, how to set the mask in setupMessageObject()

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Hi, 

I am working on F28379D device with CAN communication. Due to application's need I am using the bitfield CAN, refering to the example of C2000Ware_5_01_00_00\device_support\f2837xd\examples\cpu1\can_loopback_bitfields\cpu01\

The example code runs perfectly on the device. I noticed that the setupMessageObject() function provided in the example appears not setting mask for message filtering. (source file also attached)

//
// setupMessageObject - Setup message object as Transmit or Receive
//
void setupMessageObject(uint32_t objID, uint32_t msgID, msgObjType msgType)
{

    //
    // Use Shadow variable for IF1CMD. IF1CMD should be written to in
    // single 32-bit write.
    //
    union CAN_IF1CMD_REG CAN_IF1CMD_SHADOW;
    
    //
    // Wait for busy bit to clear.
    //
    while(CanbRegs.CAN_IF1CMD.bit.Busy)
    {
    }

    //
    // Clear and Write out the registers to program the message object.
    //
    CAN_IF1CMD_SHADOW.all = 0;    
    CanbRegs.CAN_IF1MSK.all = 0;
    CanbRegs.CAN_IF1ARB.all = 0;
    CanbRegs.CAN_IF1MCTL.all = 0;

    //
    // Set the Control, Mask, and Arb bit so that they get transferred to the
    // Message object.
    //
    CAN_IF1CMD_SHADOW.bit.Control = 1;
    CAN_IF1CMD_SHADOW.bit.Arb = 1;
    CAN_IF1CMD_SHADOW.bit.Mask = 1;
    CAN_IF1CMD_SHADOW.bit.DIR = 1;

    //
    // Set direction to transmit
    //
    if(msgType == MSG_OBJ_TYPE_TRANSMIT)
    {
        CanbRegs.CAN_IF1ARB.bit.Dir = 1;
    }

    //
    // Set Message ID (this example assumes 11 bit ID mask)
    //
    CanbRegs.CAN_IF1ARB.bit.ID = (msgID << CAN_MSG_ID_SHIFT);
    CanbRegs.CAN_IF1ARB.bit.MsgVal = 1;

    //
    // Set the data length since this is set for all transfers.  This is
    // also a single transfer and not a FIFO transfer so set EOB bit.
    //
    CanbRegs.CAN_IF1MCTL.bit.DLC = messageSize;
    CanbRegs.CAN_IF1MCTL.bit.EoB = 1;

    //
    // Transfer data to message object RAM
    //
    CAN_IF1CMD_SHADOW.bit.MSG_NUM = objID;
    CanbRegs.CAN_IF1CMD.all = CAN_IF1CMD_SHADOW.all;
}

I want to add masking for my RX message objects for my application use. It seems hard to me to find further examples of bitfield CAN examples for this device, so my best guess is like:

    //
    // Set Message ID (this example assumes 11 bit ID mask)
    //
    CanbRegs.CAN_IF1ARB.bit.ID = (msgID << CAN_MSG_ID_SHIFT);
    CanbRegs.CAN_IF1ARB.bit.MsgVal = 1;
    
    /************************** My adding here /
    // Mask setting:
    CanbRegs.CAN_IF1MSK.bit.Msk = ((uint32_t)0x7FF << CAN_MSG_ID_SHIFT);
    /*************************/

    //
    // Set the data length since this is set for all transfers.  This is
    // also a single transfer and not a FIFO transfer so set EOB bit.
    //
    CanbRegs.CAN_IF1MCTL.bit.DLC = messageSize;
    CanbRegs.CAN_IF1MCTL.bit.EoB = 1;

Could you provide advice whether that's correct way?

I tried to figure it out by debugging and setting breakpoints within the getCANMessage(uint32_t objID) function, to see whether  or not I trigger that by a incoming frame of undesired ID. But I don't know why, no matter what frame being received, undesired or desired, I couldn't get the breakpoint being hit at all.

Appreciate if you could share insights on the 2 question / issue above.

Regards,

Wei 

//###########################################################################
//
// FILE:   can_loopback_bitfields.c
//
// TITLE:  Example to demonstrate basic CAN setup and use.
//
//! \addtogroup cpu01_example_list
//! <h1>CAN External Loopback Using Bitfields (can_loopback_bitfields)</h1>
//!
//! IMPORTANT: CAN Bitfield headers require compiler v16.6.0.STS and newer!
//!
//! This example, using bitfield headers, shows the basic setup of CAN in
//! order to transmit and receive messages on the CAN bus.  The CAN
//! peripheral is configured to transmit messages with a specific CAN ID.
//! A message is then transmitted once per second, using a simple delay
//! loop for timing.  The message that is sent is a 4 byte message that
//! contains an incrementing pattern.
//!
//! This example sets up the CAN controller in External Loopback test mode.
//! Data transmitted is visible on the CAN0TX pin and can be received with
//! an appropriate mailbox configuration.
//!
//
//###########################################################################
//
// $Release Date:  $
// $Copyright:
// Copyright (C) 2013-2023 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "F28x_Project.h"

//
// Defines
//
#define CAN_MSG_ID              0x111 // This example only supports standard ID
#define CAN_TX_MSG_OBJ          1
#define CAN_RX_MSG_OBJ          2
#define CAN_MAX_BIT_DIVISOR     (13)   // The maximum CAN bit timing divisor
#define CAN_MIN_BIT_DIVISOR     (5)    // The minimum CAN bit timing divisor
#define CAN_MAX_PRE_DIVISOR     (1024) // The maximum CAN pre-divisor
#define CAN_MIN_PRE_DIVISOR     (1)    // The minimum CAN pre-divisor
#define CAN_BTR_BRP_M           (0x3F)
#define CAN_BTR_BRPE_M          (0xF0000)
#define CAN_MSG_ID_SHIFT        18U


//
// Globals
//
unsigned char ucTXMsgData[4] = {0x1, 0x2, 0x3, 0x4}; // TX Data
unsigned char ucRXMsgData[4] = {0, 0, 0, 0};         // RX Data
uint32_t messageSize = sizeof(ucTXMsgData);          // Message Size (DLC)
volatile unsigned long msgCount = 0; // A counter that keeps track of the
                                     // number of times the transmit was
                                     // successful.
volatile unsigned long errFlag = 0;  // A flag to indicate that some
                                     // transmission error occurred.

static const uint16_t canBitValues[] =
{
    0x1100, // TSEG2 2, TSEG1 2, SJW 1, Divide 5
    0x1200, // TSEG2 2, TSEG1 3, SJW 1, Divide 6
    0x2240, // TSEG2 3, TSEG1 3, SJW 2, Divide 7
    0x2340, // TSEG2 3, TSEG1 4, SJW 2, Divide 8
    0x3340, // TSEG2 4, TSEG1 4, SJW 2, Divide 9
    0x3440, // TSEG2 4, TSEG1 5, SJW 2, Divide 10
    0x3540, // TSEG2 4, TSEG1 6, SJW 2, Divide 11
    0x3640, // TSEG2 4, TSEG1 7, SJW 2, Divide 12
    0x3740  // TSEG2 4, TSEG1 8, SJW 2, Divide 13
};

typedef enum
{
        //! Transmit message object.
        MSG_OBJ_TYPE_TRANSMIT,

        //! Receive message object.
        MSG_OBJ_TYPE_RECEIVE
}
msgObjType;

//
// Function Prototypes
//
void InitCANB(void);
uint32_t setCANBitRate(uint32_t sourceClock, uint32_t bitRate);
void  setupMessageObject(uint32_t objID, uint32_t msgID, msgObjType msgType);
void sendCANMessage(uint32_t objID);
bool getCANMessage(uint32_t objID);

//
// Main
//
int
main(void)
{
    //
    // Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the F2837xD_SysCtrl.c file.
    //
    InitSysCtrl();

    //
    // Initialize GPIO:
    // This example function is found in the F2837xD_Gpio.c file and
    // illustrates how to set the GPIO to its default state.
    //
    InitGpio();
//    GPIO_SetupPinMux(30, GPIO_MUX_CPU1, 1);  //GPIO30 - CANRXA
//    GPIO_SetupPinMux(31, GPIO_MUX_CPU1, 1);  //GPIO31 - CANTXA
//    GPIO_SetupPinOptions(30, GPIO_INPUT, GPIO_ASYNC);
//    GPIO_SetupPinOptions(31, GPIO_OUTPUT, GPIO_PUSHPULL);
    GPIO_SetupPinMux(17, GPIO_MUX_CPU1, 2);  //GPIO17 - CANRXB
    GPIO_SetupPinMux(12, GPIO_MUX_CPU1, 2);  //GPIO12 - CANTXB
    GPIO_SetupPinOptions(17, GPIO_INPUT, GPIO_ASYNC);
    GPIO_SetupPinOptions(12, GPIO_OUTPUT, GPIO_PUSHPULL);

    //
    // Initialize the CAN-A controller
    //
    InitCANB();
//    InitCAN();


    //
    // Setup CAN to be clocked off the SYSCLKOUT
    //
//    ClkCfgRegs.CLKSRCCTL2.bit.CANABCLKSEL = 0;
    ClkCfgRegs.CLKSRCCTL2.bit.CANBBCLKSEL = 0;

    //
    // Set up the bit rate for the CAN bus.  This function sets up the CAN
    // bus timing for a nominal configuration.
    // In this example, the CAN bus is set to 500 kbps.
    //
    // Consult the TRM for more information about
    // CAN peripheral clocking.
    //
    uint32_t status = setCANBitRate(200000000, 500000);

    //
    // If values requested are too small or too large, catch error
    //
    if(status == 0)
    {
        errFlag++;
        ESTOP0;         // Stop here and handle error
    }

    //
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    //
    DINT;

    //
    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the F2837xD_PieCtrl.c file.
    //
    InitPieCtrl();

    //
    // Disable CPU interrupts and clear all CPU interrupt flags:
    //
    IER = 0x0000;
    IFR = 0x0000;

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in F2837xD_DefaultIsr.c.
    // This function is found in F2837xD_PieVect.c.
    //
    InitPieVectTable();

    //
    // Enable the CAN for operation.
    //
    CanbRegs.CAN_CTL.bit.Init = 0;

    //
    // Enable test mode and select external loopback
    //
//    CanbRegs.CAN_CTL.bit.Test = 1;
//    CanbRegs.CAN_TEST.bit.EXL = 1;

    //
    // Initialize the message object that will be used for sending CAN
    // messages.
    //
    setupMessageObject(CAN_TX_MSG_OBJ, CAN_MSG_ID, MSG_OBJ_TYPE_TRANSMIT);

    //
    // Initialize the message object that will be used for receiving CAN
    // messages.
    //
    setupMessageObject(CAN_RX_MSG_OBJ, CAN_MSG_ID, MSG_OBJ_TYPE_RECEIVE);

    //
    // Enter loop to send messages.  A new message will be sent once per
    // second.  The 4 bytes of message content will be treated as an unsigned
    // long and incremented by one each time.
    //
    for(;;)
    {
        //
        // Send the CAN message using object number 1 (not the same thing as
        // CAN ID, which is also 1 in this example).  This function will cause
        // the message to be transmitted right away.
        //
        sendCANMessage(CAN_TX_MSG_OBJ);

        //
        // Now wait 1 second before continuing
        //
        DELAY_US(1000*1000);

        //
        // Get the receive message
        //
        getCANMessage(CAN_RX_MSG_OBJ);

        //
        // Ensure the received data matches the transmitted data
        //
        if((ucTXMsgData[0] != ucRXMsgData[0]) ||
           (ucTXMsgData[1] != ucRXMsgData[1]) ||
           (ucTXMsgData[2] != ucRXMsgData[2]) ||
           (ucTXMsgData[3] != ucRXMsgData[3]))
        {
            errFlag++;
            asm(" ESTOP0");
        }
        else
        {
            //
            // Increment successful message count
            //
            msgCount++;
        }
            

        //
        // Increment the value in the transmitted message data.
        //
        ucTXMsgData[0] += 0x1;
        ucTXMsgData[1] += 0x1;
        ucTXMsgData[2] += 0x1;
        ucTXMsgData[3] += 0x1;
        
        //
        // Reset data if exceeds a byte
        //
        if(ucTXMsgData[0] > 0xFF)
        {
            ucTXMsgData[0] = 0;  
        }
        if(ucTXMsgData[1] > 0xFF)
        {
            ucTXMsgData[1] = 0; 
        }     
        if(ucTXMsgData[2] > 0xFF)
        {
            ucTXMsgData[2] = 0; 
        }     
        if(ucTXMsgData[3] > 0xFF)
        {
            ucTXMsgData[3] = 0; 
        } 
    }
}

void InitCANB(void)
{
    int16_t iMsg;

    //
    // Place CAN controller in init state, regardless of previous state.  This
    // will put controller in idle, and allow the message object RAM to be
    // programmed.
    //
    CanbRegs.CAN_CTL.bit.Init = 1;
    CanbRegs.CAN_CTL.bit.SWR = 1;

    //
    // Wait for busy bit to clear
    //
    while(CanbRegs.CAN_IF1CMD.bit.Busy)
    {
    }

    //
    // Clear the message value bit in the arbitration register.  This indicates
    // the message is not valid and is a "safe" condition to leave the message
    // object.  The same arb reg is used to program all the message objects.
    //
    CanbRegs.CAN_IF1CMD.bit.DIR = 1;
    CanbRegs.CAN_IF1CMD.bit.Arb = 1;
    CanbRegs.CAN_IF1CMD.bit.Control = 1;

    CanbRegs.CAN_IF1ARB.all = 0;

    CanbRegs.CAN_IF1MCTL.all = 0;

    CanbRegs.CAN_IF2CMD.bit.DIR = 1;
    CanbRegs.CAN_IF2CMD.bit.Arb = 1;
    CanbRegs.CAN_IF2CMD.bit.Control = 1;

    CanbRegs.CAN_IF2ARB.all = 0;

    CanbRegs.CAN_IF2MCTL.all = 0;

    //
    // Loop through to program all 32 message objects
    //
    for(iMsg = 1; iMsg <= 32; iMsg+=2)
    {
        //
        // Wait for busy bit to clear
        //
        while(CanbRegs.CAN_IF1CMD.bit.Busy)
        {
        }

        //
        // Initiate programming the message object
        //
        CanbRegs.CAN_IF1CMD.bit.MSG_NUM = iMsg;

        //
        // Wait for busy bit to clear
        //
        while(CanbRegs.CAN_IF2CMD.bit.Busy)
        {
        }

        //
        // Initiate programming the message object
        //
        CanbRegs.CAN_IF2CMD.bit.MSG_NUM = iMsg + 1;
    }

    //
    // Acknowledge any pending status interrupts.
    //
    volatile uint32_t discardRead = CanbRegs.CAN_ES.all;

}

//
// setCANBitRate - Set the CAN bit rate based on device clock (Hz)
//                 and desired bit rate (Hz)
//
uint32_t setCANBitRate(uint32_t sourceClock, uint32_t bitRate)
{
    uint32_t desiredRatio;
    uint32_t canBits;
    uint32_t preDivide;
    uint32_t regValue;
    uint16_t canControlValue;

    //
    // Calculate the desired clock rate.
    //
    desiredRatio = sourceClock / bitRate;

    //
    // Make sure that the Desired Ratio is not too large.  This enforces the
    // requirement that the bit rate is larger than requested.
    //
    if((sourceClock / desiredRatio) > bitRate)
    {
        desiredRatio += 1;
    }

    //
    // Check all possible values to find a matching value.
    //
    while(desiredRatio <= CAN_MAX_PRE_DIVISOR * CAN_MAX_BIT_DIVISOR)
    {
        //
        // Loop through all possible CAN bit divisors.
        //
        for(canBits = CAN_MAX_BIT_DIVISOR;
            canBits >= CAN_MIN_BIT_DIVISOR;
            canBits--)
        {
            //
            // For a given CAN bit divisor save the pre divisor.
            //
            preDivide = desiredRatio / canBits;

            //
            // If the calculated divisors match the desired clock ratio then
            // return these bit rate and set the CAN bit timing.
            //
            if((preDivide * canBits) == desiredRatio)
            {
                //
                // Start building the bit timing value by adding the bit timing
                // in time quanta.
                //
                regValue = canBitValues[canBits - CAN_MIN_BIT_DIVISOR];

                //
                // To set the bit timing register, the controller must be
                // placed
                // in init mode (if not already), and also configuration change
                // bit enabled.  The state of the register should be saved
                // so it can be restored.
                //
                canControlValue = CanbRegs.CAN_CTL.all;
                CanbRegs.CAN_CTL.bit.Init = 1;
                CanbRegs.CAN_CTL.bit.CCE = 1;

                //
                // Now add in the pre-scalar on the bit rate.
                //
                regValue |= ((preDivide - 1) & CAN_BTR_BRP_M) |
                            (((preDivide - 1) << 10) & CAN_BTR_BRPE_M);

                //
                // Set the clock bits in the and the bits of the
                // pre-scalar.
                //
                CanbRegs.CAN_BTR.all = regValue;

                //
                // Restore the saved CAN Control register.
                //
                CanbRegs.CAN_CTL.all = canControlValue;

                //
                // Return the computed bit rate.
                //
                return(sourceClock / ( preDivide * canBits));
            }
        }

        //
        // Move the divisor up one and look again.  Only in rare cases are
        // more than 2 loops required to find the value.
        //
        desiredRatio++;
    }
    return 0;
}

//
// setupMessageObject - Setup message object as Transmit or Receive
//
void setupMessageObject(uint32_t objID, uint32_t msgID, msgObjType msgType)
{

    //
    // Use Shadow variable for IF1CMD. IF1CMD should be written to in
    // single 32-bit write.
    //
    union CAN_IF1CMD_REG CAN_IF1CMD_SHADOW;
    
    //
    // Wait for busy bit to clear.
    //
    while(CanbRegs.CAN_IF1CMD.bit.Busy)
    {
    }

    //
    // Clear and Write out the registers to program the message object.
    //
    CAN_IF1CMD_SHADOW.all = 0;    
    CanbRegs.CAN_IF1MSK.all = 0;
    CanbRegs.CAN_IF1ARB.all = 0;
    CanbRegs.CAN_IF1MCTL.all = 0;

    //
    // Set the Control, Mask, and Arb bit so that they get transferred to the
    // Message object.
    //
    CAN_IF1CMD_SHADOW.bit.Control = 1;
    CAN_IF1CMD_SHADOW.bit.Arb = 1;
    CAN_IF1CMD_SHADOW.bit.Mask = 1;
    CAN_IF1CMD_SHADOW.bit.DIR = 1;

    //
    // Set direction to transmit
    //
    if(msgType == MSG_OBJ_TYPE_TRANSMIT)
    {
        CanbRegs.CAN_IF1ARB.bit.Dir = 1;
    }

    //
    // Set Message ID (this example assumes 11 bit ID mask)
    //
    CanbRegs.CAN_IF1ARB.bit.ID = (msgID << CAN_MSG_ID_SHIFT);
    CanbRegs.CAN_IF1ARB.bit.MsgVal = 1;

    //
    // Set the data length since this is set for all transfers.  This is
    // also a single transfer and not a FIFO transfer so set EOB bit.
    //
    CanbRegs.CAN_IF1MCTL.bit.DLC = messageSize;
    CanbRegs.CAN_IF1MCTL.bit.EoB = 1;

    //
    // Transfer data to message object RAM
    //
    CAN_IF1CMD_SHADOW.bit.MSG_NUM = objID;
    CanbRegs.CAN_IF1CMD.all = CAN_IF1CMD_SHADOW.all;
}

//
// sendCANMessage - Transmit data from the specified message object
//
void sendCANMessage(uint32_t objID)
{
    //
    // Use Shadow variable for IF1CMD. IF1CMD should be written to in
    // single 32-bit write.
    //
    union CAN_IF1CMD_REG CAN_IF1CMD_SHADOW;
    
    //
    // Wait for busy bit to clear.
    //
    while(CanbRegs.CAN_IF1CMD.bit.Busy)
    {
    }

    //
    // Write data to transfer into DATA-A and DATA-B interface registers
    //
    uint16_t index;
    for(index = 0; index < messageSize; index++)
    {
        switch(index)
        {
            case 0:
                CanbRegs.CAN_IF1DATA.bit.Data_0 = ucTXMsgData[index];
                break;
            case 1:
                CanbRegs.CAN_IF1DATA.bit.Data_1 = ucTXMsgData[index];
                break;
            case 2:
                CanbRegs.CAN_IF1DATA.bit.Data_2 = ucTXMsgData[index];
                break;
            case 3:
                CanbRegs.CAN_IF1DATA.bit.Data_3 = ucTXMsgData[index];
                break;
            case 4:
                CanbRegs.CAN_IF1DATB.bit.Data_4 = ucTXMsgData[index];
                break;
            case 5:
                CanbRegs.CAN_IF1DATB.bit.Data_5 = ucTXMsgData[index];
                break;
            case 6:
                CanbRegs.CAN_IF1DATB.bit.Data_6 = ucTXMsgData[index];
                break;
            case 7:
                CanbRegs.CAN_IF1DATB.bit.Data_7 = ucTXMsgData[index];
                break;
        }
    }

    //
    // Set Direction to write and set DATA-A/DATA-B to be transfered to
    // message object
    //
    CAN_IF1CMD_SHADOW.all = 0;
    CAN_IF1CMD_SHADOW.bit.DIR = 1;
    CAN_IF1CMD_SHADOW.bit.DATA_A = 1;
    CAN_IF1CMD_SHADOW.bit.DATA_B = 1;

    //
    // Set Tx Request Bit
    //
    CAN_IF1CMD_SHADOW.bit.TXRQST = 1;

    //
    // Transfer the message object to the message object specified by
    // objID.
    //
    CAN_IF1CMD_SHADOW.bit.MSG_NUM = objID;
    CanbRegs.CAN_IF1CMD.all = CAN_IF1CMD_SHADOW.all;
}

//
// getCANMessage - Check the message object for new data.
//                 If new data, data written into array and return true.
//                 If no new data, return false.
//
bool getCANMessage(uint32_t objID)
{
    bool status;
    
    //
    // Use Shadow variable for IF2CMD. IF2CMD should be written to in
    // single 32-bit write.
    //
    union CAN_IF2CMD_REG CAN_IF2CMD_SHADOW;

    //
    // Set the Message Data A, Data B, and control values to be read
    // on request for data from the message object.
    //
    CAN_IF2CMD_SHADOW.all = 0;
    CAN_IF2CMD_SHADOW.bit.Control = 1;
    CAN_IF2CMD_SHADOW.bit.DATA_A = 1;
    CAN_IF2CMD_SHADOW.bit.DATA_B = 1;

    //
    // Transfer the message object to the message object IF register.
    //
    CAN_IF2CMD_SHADOW.bit.MSG_NUM = objID;
    CanbRegs.CAN_IF2CMD.all = CAN_IF2CMD_SHADOW.all;

    //
    // Wait for busy bit to clear.
    //
    while(CanbRegs.CAN_IF2CMD.bit.Busy)
    {
    }

    //
    // See if there is new data available.
    //
    if(CanbRegs.CAN_IF2MCTL.bit.NewDat == 1)
    {
        //
        // Read out the data from the CAN registers.
        //
        uint16_t index;
        for(index = 0; index < messageSize; index++)
        {
            switch(index)
            {
                case 0:
                    ucRXMsgData[index] = CanbRegs.CAN_IF2DATA.bit.Data_0;
                break;
                case 1:
                    ucRXMsgData[index] = CanbRegs.CAN_IF2DATA.bit.Data_1;
                break;
                case 2:
                    ucRXMsgData[index] = CanbRegs.CAN_IF2DATA.bit.Data_2;
                break;
                case 3:
                    ucRXMsgData[index] = CanbRegs.CAN_IF2DATA.bit.Data_3;
                break;
                case 4:
                    ucRXMsgData[index] = CanbRegs.CAN_IF2DATB.bit.Data_4;
                break;
                case 5:
                    ucRXMsgData[index] = CanbRegs.CAN_IF2DATB.bit.Data_5;
                break;
                case 6:
                    ucRXMsgData[index] = CanbRegs.CAN_IF2DATB.bit.Data_6;
                break;
                case 7:
                    ucRXMsgData[index] = CanbRegs.CAN_IF2DATB.bit.Data_7;
                break;
            }
        }

        //
        // Populate Shadow Variable
        //
        CAN_IF2CMD_SHADOW.all = CanbRegs.CAN_IF2CMD.all;

        //
        // Clear New Data Flag
        //
        CAN_IF2CMD_SHADOW.bit.TxRqst = 1;

        //
        // Transfer the message object to the message object IF register.
        //
        CAN_IF2CMD_SHADOW.bit.MSG_NUM = objID;
        CanbRegs.CAN_IF2CMD.all = CAN_IF2CMD_SHADOW.all;

        status = true;
    }
    else
    {
        status = false;
    }

    return(status);
}

//
// End of file
//

  • Wei,

                Please take a look at C:\ti\c2000\C2000Ware_5_02_00_00\driverlib\f2837xd\examples\cpu1\can\can_ex10_mask.c. I have further explained this example in www.ti.com/lit/SPRACE5. Understand it is written using Driverlib. However, it shows how to configure the module for message object filtering. Once you understand this example, you can easily mimic the configuration in bit-field.

  • Hi Wei,

    The code you added looks ok. The MASK is used for receptance filtering, please set the MDIR bit in IF1MSK register too:

    After calling setupMessageObject(), you can check the CAN RAM manually to make sure the MASK value has been transmitted to CAN RAM correctly or not.

  • Thank you Hareesh and QJ.

    As you suggested, I've added setting of MDIR bit, and according to the tec doc sparce5, also set the UMASK bit too. ( I set these for RX objects only, cause don't care much on the TX object filtering in my application). 

    CanbRegs.CAN_IF1MSK.bit.Msk = ((uint32_t)0x7FF << CAN_MSG_ID_SHIFT);
    if(msgType == MSG_OBJ_TYPE_RECEIVE)
    {
        CanbRegs.CAN_IF1MSK.bit.MDir = 1;
        CanbRegs.CAN_IF1MCTL.bit.UMask = 1;
    }

    and the register values now looks like:


    I guess above is what suppose to have? (mask set in the way of all 1s among the effective bits for standard ID, means only exact-match of RX frame ID can pass through, that is what I want).

    Also, a question to better understand, the MDir bit means "Mask Message Direction", but I don't have a clear picture the way it function --  Does that mean, say, for a RX message object, it will ignore if you are trying to send a message from it, because the 'direction' doesn't match?  

    Appreciate for the replies.

    Regards,

    Wei

  • Hi Wei,

    I read the can.c in C2000 driverlib library of C2000Ware_5_02. The function CAN_setupMessageObject(..) configures the message MASK, so you don't need to add your own code to the function.

    The Msk is used for received messages only. The received message is stored into the message RAM if it passes the acceptance filtering. The ID field in the message object is overwritten with the ID of the received message.

    If the MDIR=0, the message direction bit (DIR) has no effect on the acceptance filtering. This means that the received message can be written to a message object whose DIR=1 (Transmit) and DIR=0 (Receive). If MDIR=1, the received message can only be written to a message object in message RAM whose DIR=0.

  • Thanks for the clarification, appreciate that.