Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Hi,
I am using PI control logic,through function DCL.h.
After debugging the code,the Duty cycle of ePWM is not changing as per the given ADC to ADCRESULT0.
Pl find below code for reference.
//###########################################################################
//
// FILE: Example_2833xEPwmDeadBand.c
//
// TITLE: ePWM Deadband Generation Example
//
//! \addtogroup f2833x_example_list
//! <h1> ePWM Deadband Generation (epwm_deadband)</h1>
//!
//! This example configures ePWM1, ePWM2 and ePWM3 for:
//! - Count up/down
//! - Deadband
//! 3 Examples are included:
//! - ePWM1: Active low PWMs
//! - ePWM2: Active low complementary PWMs
//! - ePWM3: Active high complementary PWMs
//!
//! Each ePWM is configured to interrupt on the 3rd zero event
//! when this happens the deadband is modified such that
//! 0 <= DB <= DB_MAX. That is, the deadband will move up and
//! down between 0 and the maximum value.
//!
//! \b External \b Connections \n
//! - EPWM1A is on GPIO0
//! - EPWM1B is on GPIO1
//! - EPWM2A is on GPIO2
//! - EPWM2B is on GPIO3
//! - EPWM3A is on GPIO4
//! - EPWM3B is on GPIO5
//
//
//###########################################################################
// $TI Release: $
// $Release Date: $
// $Copyright:
// Copyright (C) 2009-2023 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "DSP28x_Project.h"
// Device Headerfile and Examples Include File
#include "DCL.h"
#include "DSP2833x_Device.h"
#include "DSP2833x_Examples.h"
#include "DSP2833x_GlobalPrototypes.h"
#include "DCLF32.h"
#include "DCL_fdlog.h"
//#include "DCLC28.h"
#include "math.h"
//
// Function Prototypes
//
float rk = 20.0f;
float yk;
float lk;
float uk;
float Duty;
DCL_PI pi1 = PI_DEFAULTS;
//
// Function Prototypes
//
Uint16 LoopCount;
Uint16 ConversionCount;
void adc_isr(void);
void gpio_select(void);
void InitAdc(void);
void InitEPwm1(void);
void control_Isr(void);
float voltage1;
float cmpa;
//
// Main
//
void main(void)
{
InitSysCtrl();
DINT;
InitPieCtrl();
EALLOW;
#if (CPU_FRQ_150MHZ) // Default - 150 MHz SYSCLKOUT
//
// HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3) = 25.0 MHz
//
#define ADC_MODCLK 0x3
#endif
#if (CPU_FRQ_100MHZ)
//
// HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 100/(2*2) = 25.0 MHz
//
#define ADC_MODCLK 0x2
#endif
EDIS;
EALLOW;
SysCtrlRegs.HISPCP.all = ADC_MODCLK;
EDIS;
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.ADCINT = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
gpio_select();
InitEPwm1();
InitAdc();
PieCtrlRegs.PIEIER1.bit.INTx6 = 1;
IER |= M_INT1;
/* initialise controller variables */
pi1.Kp=2.0f;
pi1.Ki=1.0f;
pi1.Umax=0.8f;
pi1.Umin=0.2f;
rk = 20.0f; // initial value for control reference
lk = 1.0f; // control loop not saturated
//
// Enable SOCA from ePWM to start SEQ1
//
// control loop not saturated
AdcRegs.ADCMAXCONV.all = 0x0001; // Setup 2 conv's on SEQ1
AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x3; // Setup ADCINA3 as 1st SEQ1 conv.
AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x2; // Setup ADCINA2 as 2nd SEQ1 conv.
AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1;
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1; // Enable SEQ1 interrupt (every EOS)
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
for (;;) ;
}
//
// cpu_timer0_isr -
void gpio_select()
{
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0; // Enable pullup on GPIO0
GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0; // Enable pullup on GPIO0
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO0 = PWM1A
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // GPIO0 = PWM1A
EDIS;
}
void InitEPwm1()
{
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // Count up down
EPwm1Regs.TBPRD = 37500; // Set timer period
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm1Regs.TBCTR = 0x0000; // Clear counter
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0x001; // Clock ratio to SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = 000;
EPwm1Regs.TBCTL.bit.SYNCOSEL=1;
EPwm1Regs.CMPA.half.CMPA =18750; // Set compare A value
EPwm1Regs.CMPB = 18750; // Set Compare B value
EPwm1Regs.CMPCTL.bit.LOADAMODE=1;
EPwm1Regs.CMPCTL.bit.SHDWAMODE=0;
/* EPwm1Regs.DBCTL.bit.OUT_MODE=3;
EPwm1Regs.DBCTL.bit.POLSEL=2;
EPwm1Regs.DBCTL.bit.IN_MODE=0;
EPwm1Regs.DBRED=100;
EPwm1Regs.DBFED=100;*/
EPwm1Regs.AQCTLA.bit.ZRO=2; // Set PWM1A on Zero
EPwm1Regs.AQCTLA.bit.CAU=1;
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 1; // Select SOC from from CPMA on upcount
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
}
__interrupt void adc_isr(void)
{
yk=((int)AdcRegs.ADCRESULT0 >>4)*300.0f/4095.0f;
//Voltage2[ConversionCount] = AdcRegs.ADCRESULT1 >>4;
//DCL_runClamp_C1(float *data, float Umax, float Umin);
//
lk=0.0f;
uk = DCL_runPI_C2(&pi1, rk, yk);
if (uk>0.8f){
uk=0.8f;
}
else if (uk<0.1f){
uk=0.1f;
}
//uk=0.5f;
EPwm1Regs.CMPA.half.CMPA =(EPwm1Regs.TBPRD)*uk; // Set compare A value
EPwm1Regs.CMPB = EPwm1Regs.TBPRD*uk; // Set Compare B value
// If 40 conversions have been logged, start over
//
//
// Reinitialize for next ADC sequence
//
if(ConversionCount == 9)
{
ConversionCount = 0;
}
else
{
ConversionCount++;
}
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1
AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear INT SEQ1 bit
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
return;
}
Kindly resolve the issue.