It is mentioned in sec3.4 SPRS698B that GPIO19, GPIO34, GPIO35, GPIO36, GPIO37 and GPIO38 pins could glitch during power up if on chip VREG is used. Now, GPIO34 and GPIO37 are also used for boot mode selection. Will boot mode selection be affected in any way during power up, if on chip VREG is used?
In my case GPIO19 is the chip select pin for an E2PROM. Should I shift chip select to another pin?