Part Number: LAUNCHXL-F28P65X
Other Parts Discussed in Thread: UNIFLASH
Hi expert,
I'm using F28P65 LaunchPad, the issue is when I use CCS(v12.7) to program into flash there comes this error:

So, I wanted to erase the flash memory using UniFlash (v8.6.0.4688) and choosing CPU1 as this:

Seems it is erased successfully from the info of UniFlash Console. But then I ran Blank Check, the result is:

The info of Console indicates: [ERROR] C28xx_CPU1: Flash Programmer: Error during Blank Check @ address 0x00080000; expected 0xFFFFFFFF, actual 0x3EBE0048 (0)
And I still could not program into Flash.
Why is that? Is the Flash erased really successfully?
Joyce