Part Number: TMS320F28335
Dear Ti members,
I have a code that runs well and the signals are also checked on an oscilloscope which seems perfect. The code is shared below:
Original Code:
#include "DSP2833x_Device.h"
// external function prototypes
extern void InitSysCtrl(void);
extern void InitPieCtrl(void);
extern void InitPieVectTable(void);
extern void InitCpuTimers(void);
extern void ConfigCpuTimer(struct CPUTIMER_VARS *, float, float);
// Prototype statements for functions found within this file.
void Gpio_select(void);
void Setup_ePWM1(void);
void Setup_ePWM2(void);
void Setup_eCAP1(void);
interrupt void cpu_timer0_isr(void);
interrupt void eCAP1_isr(void);
// Global Variables
Uint32 PWM_Duty = 0;
Uint32 PWM_Period = 0;
Uint32 PWM2_Duty;
Uint32 PWM2_Period;
Uint32 NEW_Duty = 0;
Uint32 NEW_Period = 0;
double ref = 1.0f; // reference voltage for pid... 0.5orig
double A1 = 0;
double TPWM = (1875/2);//3750(40K),3333(45K),3000(50K),2727(55K),2500(60K),2307(65k),2143(70K),2000(75K),1875(80K),1765(85K)
//4285(35K),30K(5000).
double Kp = 0.1f; // Kp=0.5,2.993,1.0,0.5
double Ki = 0.001f;// Ki = 0.01,0,0.1,0.009,0.001
double Kd = 0.0f;// Kd = 0,0.5,0.01,1.0,0.002
double le = 0.0f; // Last or previous error
double se = 0.0f; // Cummulative error
double max = 0.49f; // max output limits for pid
double min = 0.05f; // min output limits for pid
double de; // difference of error
double e; // Current error
double updated_dutycycle =0;
double pid_out = 0;
double Duty_cycle_ratio = 0;
//###########################################################################
// main code
//###########################################################################
void main(void)
{
int counter=0; // binary counter for digital output
InitSysCtrl(); // Basic Core Init from DSP2833x_SysCtrl.c
EALLOW;
SysCtrlRegs.WDCR= 0x00AF; // Re-enable the watchdog
EDIS; // 0x00AF to NOT disable the Watchdog, Prescaler = 64
DINT; // Disable all interrupts
Gpio_select(); // GPIO9, GPIO11, GPIO34 and GPIO49 as output
// to 4 LEDs at Peripheral Explorer Board
Setup_ePWM1(); // init ePWM1A,B
Setup_ePWM2(); // init ePWM2A,B
////// START-UP CODE for 3 seconds STARTS HERE. After 3 secs, it will never run again
/// From line 70-100 ///
EPwm1Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = 1
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = 2
EPwm1Regs.TBCTL.bit.CTRMODE = 2; // up - down mode
EPwm1Regs.AQCTLA.all = 0x0060; // set ePWM1A on CMPA up
EPwm1Regs.AQCTLB.all = 0x0600; // set ePWM1B on CMPB up
EPwm1Regs.TBPRD = 1500/2; // 1KHz - PWM signal
EPwm1Regs.CMPA.half.CMPA = 750/2; // 50% duty cycle first
EPwm1Regs.CMPB = 750/2;
EPwm1Regs.DBRED = 45; // 10 microseconds delay
EPwm1Regs.DBFED = 45; // for rising and falling edge
EPwm1Regs.DBCTL.bit.OUT_MODE = 3; // ePWM1A = RED
EPwm1Regs.DBCTL.bit.POLSEL = 2; // S3=1 inverted signal at ePWM1B
EPwm1Regs.DBCTL.bit.IN_MODE = 0; // ePWM1A = source for RED & FED
EPwm2Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = 1
EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = 2
EPwm2Regs.TBCTL.bit.CTRMODE = 2; // up - down mode
EPwm2Regs.AQCTLA.all = 0x0060; // set ePWM1A on CMPA up
EPwm2Regs.AQCTLB.all = 0x0600; // set ePWM1B on CMPB up
EPwm2Regs.TBPRD = 1500/2; // 1KHz - PWM signal
EPwm2Regs.CMPA.half.CMPA = 750/2; // 50% duty cycle first
EPwm2Regs.CMPB = 750/2;
EPwm1Regs.TBCTL.bit.SYNCOSEL = 1; // generate a syncout if CTR = 0
EPwm2Regs.TBCTL.bit.PHSEN = 1; // enable phase shift for ePWM2
EPwm2Regs.TBCTL.bit.SYNCOSEL = 0; // syncin = syncout
EPwm2Regs.TBPHS.half.TBPHS = 1500/2; // 1/3 phase shift
EPwm2Regs.DBRED = 45; // 10 microseconds delay
EPwm2Regs.DBFED = 45; // for rising and falling edge
EPwm2Regs.DBCTL.bit.OUT_MODE = 3; // ePWM1A = RED
EPwm2Regs.DBCTL.bit.POLSEL = 2; // S3=1 inverted signal at ePWM1B
EPwm2Regs.DBCTL.bit.IN_MODE = 0; // ePWM1A = source for RED & FED
/// STARTUP CODE ENDS ////
Setup_eCAP1(); // init eCAP1
InitPieCtrl(); // basic setup of PIE table; from DSP2833x_PieCtrl.c
InitPieVectTable(); // default ISR's in PIE
EALLOW;
PieVectTable.TINT0 = &cpu_timer0_isr;
PieVectTable.ECAP1_INT= &eCAP1_isr;
EDIS;
InitCpuTimers(); // basic setup CPU Timer0, 1 and 2
ConfigCpuTimer(&CpuTimer0,150,100000);
PieCtrlRegs.PIEIER1.bit.INTx7 = 1; // Enable CPU Timer 0 INT
PieCtrlRegs.PIEIER4.bit.INTx1 = 1; // Enable ECAP1_INT in PIE group 4
IER |= 0x0009;
EINT;
ERTM;
CpuTimer0Regs.TCR.bit.TSS = 0; // start timer0
while(1)
{
Duty_cycle_ratio = ((double)((int32)PWM_Duty)) / 283; // This number is a ratio between 0-1
// Duty_cycle_ratio = ((double)((int32)PWM_Duty)) / TPWM); // This number is a ratio between 0-1
A1= (Duty_cycle_ratio * 3.0); // Analog Input voltage
e = (ref - A1);
se = se + e;
de = e-le;
pid_out = (Kp*e) + (Ki*se) + (Kd*de); // Pid equation
// le = e;
// if (pid_out > max)
// {
// pid_out = max;
// }
// else if (pid_out < min)
// {
// pid_out = min;
// }
updated_dutycycle = (((double)pid_out) + 0.25 );///+0.6,-1.5,0.25
// updated_dutycycle = (((double)pid_out));
if (updated_dutycycle > max)
{
updated_dutycycle = max;
}
else if (updated_dutycycle < min)
{
updated_dutycycle = min;
}
NEW_Duty = (updated_dutycycle) * TPWM;
le = e;
while(CpuTimer0.InterruptCount == 0);
CpuTimer0.InterruptCount = 0;
EALLOW;
SysCtrlRegs.WDKEY = 0x55; // service WD #1
EDIS;
counter++;
if(counter&1) GpioDataRegs.GPASET.bit.GPIO9 = 1;
else GpioDataRegs.GPACLEAR.bit.GPIO9 = 1;
if(counter&2) GpioDataRegs.GPASET.bit.GPIO11 = 1;
else GpioDataRegs.GPACLEAR.bit.GPIO11 = 1;
if(counter&4) GpioDataRegs.GPBSET.bit.GPIO34 = 1;
else GpioDataRegs.GPBCLEAR.bit.GPIO34 = 1;
if(counter&8) GpioDataRegs.GPBSET.bit.GPIO49 = 1;
else GpioDataRegs.GPBCLEAR.bit.GPIO49 = 1;
}
}
void Gpio_select(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX1.all = 0; // GPIO15 ... GPIO0 = General Puropse I/O
GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0;
GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0;
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // ePWM1A active
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // ePWM1B active
GpioCtrlRegs.GPAPUD.bit.GPIO2 = 0;
GpioCtrlRegs.GPAPUD.bit.GPIO3 = 0;
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // ePWM2A active
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // ePWM2B active
GpioCtrlRegs.GPAMUX2.all = 0; // GPIO31 ... GPIO16 = General Purpose I/O
GpioCtrlRegs.GPAPUD.bit.GPIO24= 0;
GpioCtrlRegs.GPAMUX2.bit.GPIO24= 1; // eCAP1 active
GpioCtrlRegs.GPBMUX1.all = 0; // GPIO47 ... GPIO32 = General Purpose I/O
GpioCtrlRegs.GPBMUX2.all = 0; // GPIO63 ... GPIO48 = General Purpose I/O
GpioCtrlRegs.GPCMUX1.all = 0; // GPIO79 ... GPIO64 = General Purpose I/O
GpioCtrlRegs.GPCMUX2.all = 0; // GPIO87 ... GPIO80 = General Purpose I/O
GpioCtrlRegs.GPADIR.all = 0;
GpioCtrlRegs.GPADIR.bit.GPIO9 = 1; // peripheral explorer: LED LD1 at GPIO9
GpioCtrlRegs.GPADIR.bit.GPIO11 = 1; // peripheral explorer: LED LD2 at GPIO11
GpioCtrlRegs.GPBDIR.all = 0; // GPIO63-32 as inputs
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1; // peripheral explorer: LED LD3 at GPIO34
GpioCtrlRegs.GPBDIR.bit.GPIO49 = 1; // peripheral explorer: LED LD4 at GPIO49
GpioCtrlRegs.GPCDIR.all = 0; // GPIO87-64 as inputs
EDIS;
}
void Setup_eCAP1(void)
{
//---------------------------------------------------------------------
//--- Configure eCAP1 unit for capture
//---------------------------------------------------------------------
ECap1Regs.ECEINT.all = 0; // Disable all eCAP interrupts
ECap1Regs.ECCTL1.bit.CAPLDEN = 0; // Disabled loading of capture results
ECap1Regs.ECCTL2.bit.TSCTRSTOP = 0; // Stop the counter
ECap1Regs.TSCTR = 0; // Clear the counter
ECap1Regs.CTRPHS = 0; // Clear the counter phase register
ECap1Regs.ECCTL2.all = 0x0096; // ECAP control register 2
// bit 15-11 00000: reserved
// bit 10 0: APWMPOL, don't care
// bit 9 0: CAP/APWM, 0 = capture mode, 1 = APWM mode
// bit 8 0: SWSYNC, 0 = no action (no s/w synch)
// bit 7-6 10: SYNCO_SEL, 10 = disable sync out signal
// bit 5 0: SYNCI_EN, 0 = disable Sync-In
// bit 4 1: TSCTRSTOP, 1 = enable counter
// bit 3 0: RE-ARM, 0 = don't re-arm, 1 = re-arm
// bit 2-1 11: STOP_WRAP, 11 = wrap after 4 captures
// bit 0 0: CONT/ONESHT, 0 = continuous mode
ECap1Regs.ECCTL1.all = 0x01C4; // ECAP control register 1
// bit 15-14 00: FREE/SOFT, 00 = stop TSCTR immediately
// bit 13-9 00000: PRESCALE, 00000 = divide by 1
// bit 8 1: CAPLDEN, 1 = enable capture results load
// bit 7 1: CTRRST4, 1 = reset counter on CAP4 event
// bit 6 1: CAP4POL, 0 = rising edge, 1 = falling edge
// bit 5 0: CTRRST3, 0 = do not reset counter on CAP3 event
// bit 4 0: CAP3POL, 0 = rising edge, 1 = falling edge
// bit 3 0: CTRRST2, 0 = do not reset counter on CAP2 event
// bit 2 1: CAP2POL, 0 = rising edge, 1 = falling edge
// bit 1 0: CTRRST1, 0 = do not reset counter on CAP1 event
// bit 0 0: CAP1POL, 0 = rising edge, 1 = falling edge
// ECap1Regs.ECEINT.all = 0x008; // Enable desired eCAP interrupts
ECap1Regs.ECEINT.all = 0x028; // Enable desired eCAP interrupts
// bit 15-8 0's: reserved
// bit 7 0: CTR=CMP, 0 = compare interrupt disabled
// bit 6 0: CTR=PRD, 0 = period interrupt disabled
// bit 5 0: CTROVF, 0 = overflow interrupt disabled
// bit 4 0: CEVT4, 0 = event 4 interrupt disabled
// bit 3 1: CEVT3, 1 = event 3 interrupt enabled
// bit 2 0: CEVT2, 0 = event 2 interrupt disabled
// bit 1 0: CEVT1, 0 = event 1 interrupt disabled
// bit 0 0: reserved
// ECap1Regs.ECCLR.bit.CTROVF = 1;
// ECap1Regs.ECCTL2.bit.REARM = 1;
}
interrupt void cpu_timer0_isr(void)
{
CpuTimer0.InterruptCount++;
EALLOW;
SysCtrlRegs.WDKEY = 0xAA; // service WD #2
EDIS;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
interrupt void eCAP1_isr(void)
{
ECap1Regs.ECCLR.bit.INT = 1; // Clear the ECAP1 interrupt flag
ECap1Regs.ECCLR.bit.CEVT3 = 1; // Clear the CEVT3 flag
if (ECap1Regs.ECFLG.bit.CTROVF == 1) // flag checking
{
ECap1Regs.ECCLR.bit.CTROVF = 1;
ECap1Regs.ECCTL2.bit.REARM = 1;
} else
{
// Calculate the PWM duty period (rising edge to falling edge)
PWM_Duty = (int32)ECap1Regs.CAP2 - (int32)ECap1Regs.CAP1;
// Calculate the PWM period (rising edge to rising edge)
PWM_Period = (int32)ECap1Regs.CAP3 - (int32)ECap1Regs.CAP1;
// ECap1Regs.ECCLR.bit.CTROVF = 1;
// ECap1Regs.ECCTL2.bit.REARM = 1;
EPwm1Regs.TBPRD = TPWM;
EPwm2Regs.TBPRD = TPWM;
EPwm1Regs.CMPA.half.CMPA = ((int32)NEW_Duty); // 50% duty cycle first
EPwm1Regs.CMPB = ((int32)NEW_Duty);
EPwm2Regs.CMPA.half.CMPA = ((int32)NEW_Duty); // 50% duty cycle first
EPwm2Regs.CMPB = ((int32)NEW_Duty);
EPwm1Regs.TBCTL.bit.SYNCOSEL = 1; // generate a syncout if CTR = 0
EPwm2Regs.TBCTL.bit.PHSEN = 1; // enable phase shift for ePWM2
EPwm2Regs.TBCTL.bit.SYNCOSEL = 0; // syncin = syncout
EPwm2Regs.TBPHS.half.TBPHS = TPWM; // 1/3 phase shift
}
PieCtrlRegs.PIEACK.all = PIEACK_GROUP4; // Must acknowledge the PIE group 4
}
void Setup_ePWM1(void)
{
EPwm1Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = 1
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = 2
EPwm1Regs.TBCTL.bit.CTRMODE = 2; // up - down mode
EPwm1Regs.AQCTLA.all = 0x0060; // set ePWM1A on CMPA up, clear ePWM1A on CMPA down
EPwm1Regs.AQCTLB.all = 0x0600; // set ePWM1B on CMPB up, clear ePWM1B on CMPB down
EPwm1Regs.DBRED = 55; // 10 microseconds delay
EPwm1Regs.DBFED = 55; // for rising and falling edge
EPwm1Regs.DBCTL.bit.OUT_MODE = 3; // ePWM1A = RED
EPwm1Regs.DBCTL.bit.POLSEL = 2; // S3=1 inverted signal at ePWM1B
EPwm1Regs.DBCTL.bit.IN_MODE = 0; // ePWM1A = source for RED & FED
}
void Setup_ePWM2(void)
{
EPwm2Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = 1
EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = 2
EPwm2Regs.TBCTL.bit.CTRMODE = 2; // up - down mode
EPwm2Regs.AQCTLA.all = 0x0060; // set ePWM1A on CMPA up, clear ePWM1A on CMPA down
EPwm2Regs.AQCTLB.all = 0x0600; // set ePWM1B on CMPB up, clear ePWM1B on CMPB down
EPwm2Regs.DBRED = 55; // 10 microseconds delay
EPwm2Regs.DBFED = 55; // for rising and falling edge
EPwm2Regs.DBCTL.bit.OUT_MODE = 3; // ePWM1A = RED
EPwm2Regs.DBCTL.bit.POLSEL = 2; // S3=1 inverted signal at ePWM1B
EPwm2Regs.DBCTL.bit.IN_MODE = 0; // ePWM1A = source for RED & FED
}
//===========================================================================
// End of SourceCode.
//===========================================================================
This code is run at double TPWM = (1875/2)...(Skip the startup ePWMcode). I would like to run the whole code for different TPWM values (3750/2,3333/2,3000/2,2727/2,2500/2,2307/2,2143/2,2000/2) with a delay of 1 min for each TPWM step value (3750/2,3333/2,3000/2,2727/2,2500/2,2307/2,2143/2,2000/2). I have made changes for delays like using arrays and the loop function (Line 20, 48-50,135-137,191-195,200-203) for different TPWM vaues but it is not working and also I don't see any changes in results on an oscilloscope. The purpose is to change TPWM values as mentioned above after 1 minute delay in between. Please see the changes in the code:
Changes in Code:
#include "DSP2833x_Device.h"
// external function prototypes
extern void InitSysCtrl(void);
extern void InitPieCtrl(void);
extern void InitPieVectTable(void);
extern void InitCpuTimers(void);
extern void ConfigCpuTimer(struct CPUTIMER_VARS *, float, float);
// Prototype statements for functions found within this file.
void Gpio_select(void);
void Setup_ePWM1(void);
void Setup_ePWM2(void);
void Setup_eCAP1(void);
interrupt void cpu_timer0_isr(void);
interrupt void eCAP1_isr(void);
void delay_minutes(float minutes);
// Global Variables
Uint32 PWM_Duty = 0;
Uint32 PWM_Period = 0;
Uint32 PWM2_Duty;
Uint32 PWM2_Period;
Uint32 NEW_Duty = 0;
Uint32 NEW_Period = 0;
double ref = 1.0f; // reference voltage for pid... 0.5orig
double A1 = 0;
double TPWM = (1875/2);//3750(40K),3333(45K),3000(50K),2727(55K),2500(60K),2307(65k),2143(70K),2000(75K),1875(80K),1765(85K)
//4285(35K),30K(5000).
double Kp = 0.1f; // Kp=0.5,2.993,1.0,0.5
double Ki = 0.001f;// Ki = 0.01,0,0.1,0.009,0.001
double Kd = 0.0f;// Kd = 0,0.5,0.01,1.0,0.002
double le = 0.0f; // Last or previous error
double se = 0.0f; // Cummulative error
double max = 0.49f; // max output limits for pid
double min = 0.05f; // min output limits for pid
double de; // difference of error
double e; // Current error
double updated_dutycycle =0;
double pid_out = 0;
double Duty_cycle_ratio = 0;
Uint32 TPWM_values[] = {3750/2, 3333/2, 3000/2, 2727/2, 2500/2, 2307/2, 2143/2, 2000/2};
Uint32 num_TPWM_values = sizeof(TPWM_values) / sizeof(TPWM_values[0]);
Uint32 k;
//###########################################################################
// main code
//###########################################################################
void main(void)
{
int counter=0; // binary counter for digital output
InitSysCtrl(); // Basic Core Init from DSP2833x_SysCtrl.c
EALLOW;
SysCtrlRegs.WDCR= 0x00AF; // Re-enable the watchdog
EDIS; // 0x00AF to NOT disable the Watchdog, Prescaler = 64
DINT; // Disable all interrupts
Gpio_select(); // GPIO9, GPIO11, GPIO34 and GPIO49 as output
// to 4 LEDs at Peripheral Explorer Board
Setup_ePWM1(); // init ePWM1A,B
Setup_ePWM2(); // init ePWM2A,B
////// START-UP CODE for 3 seconds STARTS HERE. After 3 secs, it will never run again
/// From line 70-100 ///
EPwm1Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = 1
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = 2
EPwm1Regs.TBCTL.bit.CTRMODE = 2; // up - down mode
EPwm1Regs.AQCTLA.all = 0x0060; // set ePWM1A on CMPA up
EPwm1Regs.AQCTLB.all = 0x0600; // set ePWM1B on CMPB up
EPwm1Regs.TBPRD = 1500/2; // 1KHz - PWM signal
EPwm1Regs.CMPA.half.CMPA = 750/2; // 50% duty cycle first
EPwm1Regs.CMPB = 750/2;
EPwm1Regs.DBRED = 45; // 10 microseconds delay
EPwm1Regs.DBFED = 45; // for rising and falling edge
EPwm1Regs.DBCTL.bit.OUT_MODE = 3; // ePWM1A = RED
EPwm1Regs.DBCTL.bit.POLSEL = 2; // S3=1 inverted signal at ePWM1B
EPwm1Regs.DBCTL.bit.IN_MODE = 0; // ePWM1A = source for RED & FED
EPwm2Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = 1
EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = 2
EPwm2Regs.TBCTL.bit.CTRMODE = 2; // up - down mode
EPwm2Regs.AQCTLA.all = 0x0060; // set ePWM1A on CMPA up
EPwm2Regs.AQCTLB.all = 0x0600; // set ePWM1B on CMPB up
EPwm2Regs.TBPRD = 1500/2; // 1KHz - PWM signal
EPwm2Regs.CMPA.half.CMPA = 750/2; // 50% duty cycle first
EPwm2Regs.CMPB = 750/2;
EPwm1Regs.TBCTL.bit.SYNCOSEL = 1; // generate a syncout if CTR = 0
EPwm2Regs.TBCTL.bit.PHSEN = 1; // enable phase shift for ePWM2
EPwm2Regs.TBCTL.bit.SYNCOSEL = 0; // syncin = syncout
EPwm2Regs.TBPHS.half.TBPHS = 1500/2; // 1/3 phase shift
EPwm2Regs.DBRED = 45; // 10 microseconds delay
EPwm2Regs.DBFED = 45; // for rising and falling edge
EPwm2Regs.DBCTL.bit.OUT_MODE = 3; // ePWM1A = RED
EPwm2Regs.DBCTL.bit.POLSEL = 2; // S3=1 inverted signal at ePWM1B
EPwm2Regs.DBCTL.bit.IN_MODE = 0; // ePWM1A = source for RED & FED
/// STARTUP CODE ENDS ////
Setup_eCAP1(); // init eCAP1
InitPieCtrl(); // basic setup of PIE table; from DSP2833x_PieCtrl.c
InitPieVectTable(); // default ISR's in PIE
EALLOW;
PieVectTable.TINT0 = &cpu_timer0_isr;
PieVectTable.ECAP1_INT= &eCAP1_isr;
EDIS;
InitCpuTimers(); // basic setup CPU Timer0, 1 and 2
ConfigCpuTimer(&CpuTimer0,150,100000);
PieCtrlRegs.PIEIER1.bit.INTx7 = 1; // Enable CPU Timer 0 INT
PieCtrlRegs.PIEIER4.bit.INTx1 = 1; // Enable ECAP1_INT in PIE group 4
IER |= 0x0009;
EINT;
ERTM;
CpuTimer0Regs.TCR.bit.TSS = 0; // start timer0
for (k = 0; k < num_TPWM_values; k++)
{
TPWM = TPWM_values[k];
while(1)
{
Duty_cycle_ratio = ((double)((int32)PWM_Duty)) / 283; // This number is a ratio between 0-1
// Duty_cycle_ratio = ((double)((int32)PWM_Duty)) / TPWM); // This number is a ratio between 0-1
A1= (Duty_cycle_ratio * 3.0); // Analog Input voltage
e = (ref - A1);
se = se + e;
de = e-le;
pid_out = (Kp*e) + (Ki*se) + (Kd*de); // Pid equation
// le = e;
// if (pid_out > max)
// {
// pid_out = max;
// }
// else if (pid_out < min)
// {
// pid_out = min;
// }
updated_dutycycle = (((double)pid_out) + 0.25 );///+0.6,-1.5,0.25
// updated_dutycycle = (((double)pid_out));
if (updated_dutycycle > max)
{
updated_dutycycle = max;
}
else if (updated_dutycycle < min)
{
updated_dutycycle = min;
}
NEW_Duty = (updated_dutycycle) * TPWM;
le = e;
while(CpuTimer0.InterruptCount == 0);
CpuTimer0.InterruptCount = 0;
EALLOW;
SysCtrlRegs.WDKEY = 0x55; // service WD #1
EDIS;
counter++;
if(counter&1) GpioDataRegs.GPASET.bit.GPIO9 = 1;
else GpioDataRegs.GPACLEAR.bit.GPIO9 = 1;
if(counter&2) GpioDataRegs.GPASET.bit.GPIO11 = 1;
else GpioDataRegs.GPACLEAR.bit.GPIO11 = 1;
if(counter&4) GpioDataRegs.GPBSET.bit.GPIO34 = 1;
else GpioDataRegs.GPBCLEAR.bit.GPIO34 = 1;
if(counter&8) GpioDataRegs.GPBSET.bit.GPIO49 = 1;
else GpioDataRegs.GPBCLEAR.bit.GPIO49 = 1;
if (CpuTimer0.InterruptCount >= 60000000) // Check if 1 minute has elapsed
{
CpuTimer0.InterruptCount = 0;
break;
}
}
}
}
void delay_minutes(float minutes)
{
for (k = 0; k < (minutes * 60000000); k++);
}
void Gpio_select(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX1.all = 0; // GPIO15 ... GPIO0 = General Puropse I/O
GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0;
GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0;
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // ePWM1A active
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // ePWM1B active
GpioCtrlRegs.GPAPUD.bit.GPIO2 = 0;
GpioCtrlRegs.GPAPUD.bit.GPIO3 = 0;
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // ePWM2A active
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // ePWM2B active
GpioCtrlRegs.GPAMUX2.all = 0; // GPIO31 ... GPIO16 = General Purpose I/O
GpioCtrlRegs.GPAPUD.bit.GPIO24= 0;
GpioCtrlRegs.GPAMUX2.bit.GPIO24= 1; // eCAP1 active
GpioCtrlRegs.GPBMUX1.all = 0; // GPIO47 ... GPIO32 = General Purpose I/O
GpioCtrlRegs.GPBMUX2.all = 0; // GPIO63 ... GPIO48 = General Purpose I/O
GpioCtrlRegs.GPCMUX1.all = 0; // GPIO79 ... GPIO64 = General Purpose I/O
GpioCtrlRegs.GPCMUX2.all = 0; // GPIO87 ... GPIO80 = General Purpose I/O
GpioCtrlRegs.GPADIR.all = 0;
GpioCtrlRegs.GPADIR.bit.GPIO9 = 1; // peripheral explorer: LED LD1 at GPIO9
GpioCtrlRegs.GPADIR.bit.GPIO11 = 1; // peripheral explorer: LED LD2 at GPIO11
GpioCtrlRegs.GPBDIR.all = 0; // GPIO63-32 as inputs
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1; // peripheral explorer: LED LD3 at GPIO34
GpioCtrlRegs.GPBDIR.bit.GPIO49 = 1; // peripheral explorer: LED LD4 at GPIO49
GpioCtrlRegs.GPCDIR.all = 0; // GPIO87-64 as inputs
EDIS;
}
void Setup_eCAP1(void)
{
//---------------------------------------------------------------------
//--- Configure eCAP1 unit for capture
//---------------------------------------------------------------------
ECap1Regs.ECEINT.all = 0; // Disable all eCAP interrupts
ECap1Regs.ECCTL1.bit.CAPLDEN = 0; // Disabled loading of capture results
ECap1Regs.ECCTL2.bit.TSCTRSTOP = 0; // Stop the counter
ECap1Regs.TSCTR = 0; // Clear the counter
ECap1Regs.CTRPHS = 0; // Clear the counter phase register
ECap1Regs.ECCTL2.all = 0x0096; // ECAP control register 2
// bit 15-11 00000: reserved
// bit 10 0: APWMPOL, don't care
// bit 9 0: CAP/APWM, 0 = capture mode, 1 = APWM mode
// bit 8 0: SWSYNC, 0 = no action (no s/w synch)
// bit 7-6 10: SYNCO_SEL, 10 = disable sync out signal
// bit 5 0: SYNCI_EN, 0 = disable Sync-In
// bit 4 1: TSCTRSTOP, 1 = enable counter
// bit 3 0: RE-ARM, 0 = don't re-arm, 1 = re-arm
// bit 2-1 11: STOP_WRAP, 11 = wrap after 4 captures
// bit 0 0: CONT/ONESHT, 0 = continuous mode
ECap1Regs.ECCTL1.all = 0x01C4; // ECAP control register 1
// bit 15-14 00: FREE/SOFT, 00 = stop TSCTR immediately
// bit 13-9 00000: PRESCALE, 00000 = divide by 1
// bit 8 1: CAPLDEN, 1 = enable capture results load
// bit 7 1: CTRRST4, 1 = reset counter on CAP4 event
// bit 6 1: CAP4POL, 0 = rising edge, 1 = falling edge
// bit 5 0: CTRRST3, 0 = do not reset counter on CAP3 event
// bit 4 0: CAP3POL, 0 = rising edge, 1 = falling edge
// bit 3 0: CTRRST2, 0 = do not reset counter on CAP2 event
// bit 2 1: CAP2POL, 0 = rising edge, 1 = falling edge
// bit 1 0: CTRRST1, 0 = do not reset counter on CAP1 event
// bit 0 0: CAP1POL, 0 = rising edge, 1 = falling edge
// ECap1Regs.ECEINT.all = 0x008; // Enable desired eCAP interrupts
ECap1Regs.ECEINT.all = 0x028; // Enable desired eCAP interrupts
// bit 15-8 0's: reserved
// bit 7 0: CTR=CMP, 0 = compare interrupt disabled
// bit 6 0: CTR=PRD, 0 = period interrupt disabled
// bit 5 0: CTROVF, 0 = overflow interrupt disabled
// bit 4 0: CEVT4, 0 = event 4 interrupt disabled
// bit 3 1: CEVT3, 1 = event 3 interrupt enabled
// bit 2 0: CEVT2, 0 = event 2 interrupt disabled
// bit 1 0: CEVT1, 0 = event 1 interrupt disabled
// bit 0 0: reserved
// ECap1Regs.ECCLR.bit.CTROVF = 1;
// ECap1Regs.ECCTL2.bit.REARM = 1;
}
interrupt void cpu_timer0_isr(void)
{
CpuTimer0.InterruptCount++;
EALLOW;
SysCtrlRegs.WDKEY = 0xAA; // service WD #2
EDIS;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
interrupt void eCAP1_isr(void)
{
ECap1Regs.ECCLR.bit.INT = 1; // Clear the ECAP1 interrupt flag
ECap1Regs.ECCLR.bit.CEVT3 = 1; // Clear the CEVT3 flag
if (ECap1Regs.ECFLG.bit.CTROVF == 1) // flag checking
{
ECap1Regs.ECCLR.bit.CTROVF = 1;
ECap1Regs.ECCTL2.bit.REARM = 1;
} else
{
// Calculate the PWM duty period (rising edge to falling edge)
PWM_Duty = (int32)ECap1Regs.CAP2 - (int32)ECap1Regs.CAP1;
// Calculate the PWM period (rising edge to rising edge)
PWM_Period = (int32)ECap1Regs.CAP3 - (int32)ECap1Regs.CAP1;
// ECap1Regs.ECCLR.bit.CTROVF = 1;
// ECap1Regs.ECCTL2.bit.REARM = 1;
EPwm1Regs.TBPRD = TPWM;
EPwm2Regs.TBPRD = TPWM;
EPwm1Regs.CMPA.half.CMPA = ((int32)NEW_Duty); // 50% duty cycle first
EPwm1Regs.CMPB = ((int32)NEW_Duty);
EPwm2Regs.CMPA.half.CMPA = ((int32)NEW_Duty); // 50% duty cycle first
EPwm2Regs.CMPB = ((int32)NEW_Duty);
EPwm1Regs.TBCTL.bit.SYNCOSEL = 1; // generate a syncout if CTR = 0
EPwm2Regs.TBCTL.bit.PHSEN = 1; // enable phase shift for ePWM2
EPwm2Regs.TBCTL.bit.SYNCOSEL = 0; // syncin = syncout
EPwm2Regs.TBPHS.half.TBPHS = TPWM; // 1/3 phase shift
}
PieCtrlRegs.PIEACK.all = PIEACK_GROUP4; // Must acknowledge the PIE group 4
}
void Setup_ePWM1(void)
{
EPwm1Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = 1
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = 2
EPwm1Regs.TBCTL.bit.CTRMODE = 2; // up - down mode
EPwm1Regs.AQCTLA.all = 0x0060; // set ePWM1A on CMPA up, clear ePWM1A on CMPA down
EPwm1Regs.AQCTLB.all = 0x0600; // set ePWM1B on CMPB up, clear ePWM1B on CMPB down
EPwm1Regs.DBRED = 55; // 10 microseconds delay
EPwm1Regs.DBFED = 55; // for rising and falling edge
EPwm1Regs.DBCTL.bit.OUT_MODE = 3; // ePWM1A = RED
EPwm1Regs.DBCTL.bit.POLSEL = 2; // S3=1 inverted signal at ePWM1B
EPwm1Regs.DBCTL.bit.IN_MODE = 0; // ePWM1A = source for RED & FED
}
void Setup_ePWM2(void)
{
EPwm2Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = 1
EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = 2
EPwm2Regs.TBCTL.bit.CTRMODE = 2; // up - down mode
EPwm2Regs.AQCTLA.all = 0x0060; // set ePWM1A on CMPA up, clear ePWM1A on CMPA down
EPwm2Regs.AQCTLB.all = 0x0600; // set ePWM1B on CMPB up, clear ePWM1B on CMPB down
EPwm2Regs.DBRED = 55; // 10 microseconds delay
EPwm2Regs.DBFED = 55; // for rising and falling edge
EPwm2Regs.DBCTL.bit.OUT_MODE = 3; // ePWM1A = RED
EPwm2Regs.DBCTL.bit.POLSEL = 2; // S3=1 inverted signal at ePWM1B
EPwm2Regs.DBCTL.bit.IN_MODE = 0; // ePWM1A = source for RED & FED
}
//===========================================================================
// End of SourceCode.
//===========================================================================
Please suggest and rectify in the change code for my requirements.
Thanks
Kind Regards
Arsalan