This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28027 eCAP count error when measuring external pulse period

Hello,

I'm practicing with 28027 with its eCap function, using "Example_2802xECap_Capture_Pwm" sample project (along with TI's 2802x header files and examples package). In this example, it use ePWM3 to generate a PWM output on GPIO4, and measures GPIO4's output pulse via eCap1 on GPIO19, and the captured values in CAP1~CAP4 is very accurate -- exactly the same as what the PWM's settings. However, when I attempted to make use of eCap1 to captuer an external 32k signal (CMOS output, squre wave), the captured values in CAP1~CAP4 varies a lot around 1831, not exactly a fixed count!  What may be the reason? I have tried over 2 more days, but without any progress, hope you can shed me some light on this.

Thank you very much.

Li dongsheng.

Below is the code for init.

void InitECapture()
{
   ECap1Regs.ECEINT.all = 0x0000;             // Disable all capture interrupts
   ECap1Regs.ECCLR.all = 0xFFFF;              // Clear all CAP interrupt flags
   ECap1Regs.ECCTL1.bit.CAPLDEN = 0;          // Disable CAP1-CAP4 register loads
   ECap1Regs.ECCTL2.bit.TSCTRSTOP = 0;        // Make sure the counter is stopped

   // Configure peripheral registers
   ECap1Regs.ECCTL2.bit.CONT_ONESHT = 1;      // One-shot
   ECap1Regs.ECCTL2.bit.STOP_WRAP = 3;        // Stop at 4 events
   ECap1Regs.ECCTL1.bit.CAP1POL = 0;          // Rising edge
   ECap1Regs.ECCTL1.bit.CAP2POL = 0;          // Rising edge
   ECap1Regs.ECCTL1.bit.CAP3POL = 0;          // Rising edge
   ECap1Regs.ECCTL1.bit.CAP4POL = 0;          // Rising edge
   ECap1Regs.ECCTL1.bit.CTRRST1 = 1;          // Difference operation
   ECap1Regs.ECCTL1.bit.CTRRST2 = 1;          // Difference operation
   ECap1Regs.ECCTL1.bit.CTRRST3 = 1;          // Difference operation
   ECap1Regs.ECCTL1.bit.CTRRST4 = 1;          // Difference operation
   ECap1Regs.ECCTL2.bit.SYNCI_EN = 0;         // Disable sync in
   ECap1Regs.ECCTL2.bit.SYNCO_SEL = 0;        // Pass through
   ECap1Regs.ECCTL1.bit.CAPLDEN = 1;          // Enable capture units

   ECap1Regs.ECCTL2.bit.TSCTRSTOP = 1;        // Start Counter
   ECap1Regs.ECCTL2.bit.REARM = 1;            // arm one-shot
   ECap1Regs.ECCTL1.bit.CAPLDEN = 1;          // Enable CAP1-CAP4 register loads
   ECap1Regs.ECEINT.bit.CEVT4 = 1;            // 4 events = interrupt

}

void InitECap1Gpio(void)
{
   EALLOW;
/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.

// GpioCtrlRegs.GPAPUD.bit.GPIO5 = 0;      // Enable pull-up on GPIO5 (CAP1)
   GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0;     // Enable pull-up on GPIO19 (CAP1)

// Inputs are synchronized to SYSCLKOUT by default.
// Comment out other unwanted lines.

// GpioCtrlRegs.GPAQSEL1.bit.GPIO5 = 0;    // Synch to SYSCLKOUT GPIO5 (CAP1)
   GpioCtrlRegs.GPAQSEL2.bit.GPIO19 = 0;   // Synch to SYSCLKOUT GPIO19 (CAP1)

/* Configure eCAP-1 pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be eCAP1 functional pins.
// Comment out other unwanted lines.

// GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 3;     // Configure GPIO5 as CAP1
   GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 3;    // Configure GPIO19 as CAP1

    EDIS;
}