Part Number: TMDXIDDK379D
Hi,
Ti friends!
Recently, while using the code that accompanies the kit, confusion arose about the SDFM trigger source. The main points are as follows:
1. The code explains that pwm10 is used to passover pwm1 sync to pwm11 for SDFM sync, but in the code pwm10 has not been configured in any way, and I do not see any connection between him and pwm11, so how does it achieve synchronisation?

2. PWM11.CMPC, PWM11.CMPD, PWM12.CMPC and PWM12.CMPD signals cannot synchronize the filters. This option is not being used in this example.
How do I understand this statement, is it because synchronous triggering is not possible, but rather they can only reset the SINC3 filter in hardware?

Thanks for your help!