Part Number: TMS320F28386D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi !
I'm using 28386D and tying to using IPC. but stil i have an error
when i initialize DSP with code that
#ifdef _FLASH
Device_bootCPU2(BOOTMODE_BOOT_TO_FLASH_SECTOR0);
#else
Device_bootCPU2(BOOTMODE_BOOT_TO_M0RAM);
#endif
-------------------------------------------------------------
<Linking>
undefined first referenced
symbol in file
--------- ----------------
IPC_Instance ./SOURCE_FILE/Base/device.obj
SysCtl_controlCPU2Reset ./SOURCE_FILE/Base/device.obj
i have an error when i bulld, but without that code there is no error.
could somebody help us?
<Linking>
undefined first referenced
symbol in file
--------- ----------------
IPC_Instance ./SOURCE_FILE/Base/device.obj
SysCtl_controlCPU2Reset ./SOURCE_FILE/Base/device.obj