This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039: TMS320F280039C: Break at address "0x3fdba4" with no debug information available, or outside of program code.

Part Number: TMS320F280039
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hello,

I am using Code Composer Studio 12.6.0.00008 along with C2000Ware_MotorControl_SDK_4_01_00_00. I am using the 280039C  processor in my customized board. Whenever i try to flash the program, it gives me the message: Break at address "0x3fdba4" with no debug information available, or outside of program code. It is getting stuck at the Stack pointer. I did not face this issue before. For some reason, I had to reinstall code composer studio since i was using version 12.0.0 version before. After installing 12.6.0, I imported our project and tried flashing but failed because of the above reason mentioned. The exact same project gets flashed through my colleague's laptop(he is using the same CCS version and same Motor Control SDK, everything else such as the include options and other settings are similar). I am wondering what could be the potential reason!!