Part Number: TMS320F28379D
Tool/software:
Hello I am new to TI's MCUs and I am trying to receive a CAN message being sent from a MCP 2515 using the program below. I was sure to define the _LAUNCHXL_F28379D to my predefined symbols and I have attached relevant code and a copy of my .syscfg file below. I have tried looking at the debugging tips provided in sprace5a; however, I have not been able to find anything that may resolve my issue. Help would be greatly appreciated.
//
// Included Files
//
#include "board.h"
#include "c2000ware_libraries.h"
volatile unsigned int recievedData = 0;
//
// Main
//
void main(void)
{
//
// Initialize device clock and peripherals
//
Device_init();
//
// Disable pin locks and enable internal pull-ups.
//
Device_initGPIO();
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// PinMux and Peripheral Initialization
//
Board_init();
//
// C2000Ware Library initialization
//
C2000Ware_libraries_init();
//
// Enable Global Interrupt (INTM) and real time interrupt (DBGM)
//
EINT;
ERTM;
CAN_startModule(myCAN0_BASE);
uint16_t rxMsgData[8];
while(1)
{
if (CAN_readMessage(myCAN0_BASE, 2, rxMsgData))
recievedData = 1;
}
}
//
// End of File
//