Tool/software:
Hello all,
Reading all over the forum and being confused about the clock design on F28388D control card where two clocks of 20MHz and 25MHz are used since the USB boot loader needs the 20MHz as it's hardcoded for that clock( why? ) and for EtherCAT compatibility the 25MHz is needed to be compliant ( I'm already crying ....)
So, how to simplify this for us? Can I use only a 20MHz clock on our design to be able to use the USB bootloader and at the same time use EtherCAT safely? what are the challenges if we use a 20MHz clock with EtherCAT instead of 25MHz?
Thanks
John