Part Number: TMS320F28388D
Tool/software:
I want to connect 28388d and 280036C in daisy chain method and debug two MCUs using one debugger (xds200i).
First, the circuit I connected is as follows.
emu0 and emu1 and TCK_RET are not connected. (If this is a problem, please let me know)

First, when I made a test connection, it said it was successful. This probably means there is no problem with the hardware connection.

the problem is
The .out file of 28388d is loaded properly and appears as shown below. However, 280036c does not seem to be loading.

I think there are separate .out files for 28388d and 280036c, but I don't seem to know how to load them.
To summarize, I have set up hardware debugging of two MCUs with one debugger, but I want to debug them by loading each .out file. I would appreciate it if you could tell me the procedure and method.
First of all, below is my debugging settings.