This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386D: Boot Mode

Expert 2470 points

Part Number: TMS320F28386D

Tool/software:

When set BOOTPIN_CONFIG  and BOOTDEF as below example.

One question about the GPIO pin voltage level mapping relationship to Boot Mode.

When GPIO2 = 1, GPIO1 = 0, GPIO0 =1,  does it mean boot mode table number 5 (USB Boot)?

When GPIO2 = 1, GPIO1 = 0, GPIO0 =0,  does it mean boot mode table number 4 (Flash Boot)?

  • Hi,

    One question about the GPIO pin voltage level mapping relationship to Boot Mode.

    When GPIO2 = 1, GPIO1 = 0, GPIO0 =1,  does it mean boot mode table number 5 (USB Boot)?

    When GPIO2 = 1, GPIO1 = 0, GPIO0 =0,  does it mean boot mode table number 4 (Flash Boot)?

    This is correct.

    Best Regards,

    Ben Collier