Part Number: TMS320F28P550SJ
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi,
What should be the cause of the error below:
First stage, loading the kernel, went without error.
82==82
fe==fe
6==6
0==0
0==0
0==0
Bit rate /s of transfer was: 7647.001953
Kernel loaded! Booting kernel...
Done waiting for kernel boot...
Attempting autobaud to send function message...
What operation do you want to perform?
1-DFU CPU1
2-Erase CPU1
3-Verify CPU1
4-Unlock CPU1 Zone 1
5-Unlock CPU1 Zone 2
6-Run CPU1
7-Reset CPU1
0-DONE
Second stage, DFU CPU1. Error 0x83198 occurred.
6
0
1
9a
6
0
6
0
0
0
Bit rate /s of transfer was: 29686.691406
Application load successful!
Done waiting for application to download and boot...
SUCCESS of Command
ERROR Status: PROGRAM_ERROR
ERROR Address: 0x83198
Flash API Error: Invalid Address
Please refer to the Flash API documentation for further explanation of the error.
FMSTAT Register contents: 00
What operation do you want to perform?
1-DFU CPU1
2-Erase CPU1
3-Verify CPU1
4-Unlock CPU1 Zone 1
5-Unlock CPU1 Zone 2
6-Run CPU1
7-Reset CPU1
0-DONE