Other Parts Discussed in Thread: ISO1050
Tool/software:
Hello all,
Just started to work with IDDK on the CAN bus, after not receiving anything from the board, it seemed there is a hardware issue, as can be seen, the CAN_TX and CAN_RX are swapped at the schematic level ( never do this please :((( ) , then to the ISO1050 we have a wrong connection of CANTX and CANRX subsequently , do you confirm this or I'm missing something here ( I hope not :) )
I'm sending dummy packets to the CANTX, but I see nothing, it seems ISO1050 doesn't like inputs at its output
ISO1050 datasheet:
and of course, the symbols are self-explanatory:
do you confirm this? Shall I proceed with the re-work and swap those connections somehow?
John