This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386D: Cannot import the project

Expert 2480 points

Part Number: TMS320F28386D
Other Parts Discussed in Thread: C2000WARE

Tool/software:

When I changed the boot_ex1_cpu1_cpu2_cm_secure_flash.projectspec to add the below two files into build.

dcsm.asm and dcsm.cmd from example dcsm_security_tool

The only changed part as compared windows shows.

Then when import the project into workspace, there is no project I can select now.

Why this happen?

C:\ti\c2000\C2000Ware_5_02_00_00\driverlib\f2838x\examples\c28x\boot\CCS