This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Two questions about TMS320F28027PT

Other Parts Discussed in Thread: TMS320F28027

Dear Friends

I had two questions about TMS320F28027:

1. From the C2000 PSG, it shows that the F28027 has 9 channels PWM, but from the datasheet, I only found 8 channels(P28,P29,P37~P42)

    Which is right? I want to know it.

   If it has 9 channels, which Pin is the 9th channel?

 

2. If only use Internal Zero-pin Oscillators, is it can work normally?

    The frequency is 10 MHz ± 1% or better ?

 

Thanks for your kindly help.