This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: TMS320F280049C

Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE,

Tool/software:

Hello,
I use the TMS320F280049C in conjunction with the CCS v12. The is07 project of the C2000Ware_MotorControl_SDK_5_02_00_00 serves as the basis for my project. So I can load the application into the flash using CCS. After switching off and on again, the application boots as desired - so far everything is fine. Is it possible to delete the burnt application from the flash without flashing a new version - I want to reset the flash memory default state?

Best regards