Part Number: TMS320F280039C
Tool/software:
Hi,TI expert:
I configured the software project using 280039c, and configured DCSM, enable the password lock, and then I burned the project into a new DSP, tried many times, and every time it was the same phenomenon: after using the out file for the first time, an error would be reported, and the DSP found that only the password could be displayed, and the other flash and OTP data were 0, that is, the locked state; In this case, the program is running abnormally, you need to connect again, after decrypting and burning the out file again, the password is completely locked, and then the program will run normally, what is the reason?
the first time download error is:

the first time, password didn't lock

but flash data is locked