Part Number: TMS320F28035
Tool/software:
Hi experts,
My customer is seeing spike at COMP2A pin like the following:

The frequency of the spike is same to the ADC trigger frequency. Is seems the spike is somehow connected to ADC, therefore we tried to remove some of the SOC. It turns out when we remove SOC1(A2) and SOC8(B4), the spike waveform changes. Removing A2 or B4 SOC would remove the spike at the comp2A pin too:
(Removing B4)
(Removing A2)
If both A2 and B4 SOC are removed, there is no spike
(Removing both A2 and B4)
After removing all SOCs but A2 and B4, there are still spikes but the waveform is different:

Any idea where the spike come from?
Comp2A is connected to COMP1B externally, capacitor on COMP2A pin is 3.3pF, capacitor on ADCs is around 2nF.
Regards,
Hang.