Part Number: TMS320F280034-Q1
Tool/software:
Just want to make sure I am using a valid boot configuration to enable boot over SCI. I am utilizing GPIO pins 2 & 3 for the SCI interface. The pins will also be used for serial communication after boot. GPIO24 has a pull up to 3.3V and is connected to a connector pin so that we can pull it low to enable serial boot.