Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Tool/software:
Hello,
I am working on a FreeRTOS project using the f28379d microcontroller. When I try to add FreeRTOS to this project using Sysconfig, I get the error shown in the attached code snipped.
"../2837xD_RAM_lnk_cpu1.cmd", line 80: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment/blocking fails for section ".text" size 0x24c2 page 0. Available memory ranges: RAMD0 size: 0x800 unused: 0x0 max hole: 0x0 RAMLS0 size: 0x800 unused: 0x0 max hole: 0x0 RAMLS1 size: 0x800 unused: 0x1 max hole: 0x1 RAMLS2 size: 0x800 unused: 0x660 max hole: 0x660 RAMLS3 size: 0x800 unused: 0x800 max hole: 0x800 RAMLS4 size: 0x800 unused: 0x800 max hole: 0x800 error #10010: errors encountered during linking; "empty_sysconfig_337zwt2.out" not built
My .cmd file.
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002
RAMM0 : origin = 0x000123, length = 0x0002DD
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS_ALL : origin = 0x008000, length = 0x002800 // added for freertos
// RAMLS0 : origin = 0x008000, length = 0x000800
// RAMLS1 : origin = 0x008800, length = 0x000800
// RAMLS2 : origin = 0x009000, length = 0x000800
// RAMLS3 : origin = 0x009800, length = 0x000800
// RAMLS4 : origin = 0x00A000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x001FF0 /* on-chip Flash */
// FLASHN_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x000121 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
// RAMGS11 : origin = 0x017000, length = 0x000FF8 /* Uncomment for F28374D, F28376D devices */
// RAMGS11_RSVD : origin = 0x017FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMGS11 : origin = 0x017000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS12 : origin = 0x018000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS13 : origin = 0x019000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS15 : origin = 0x01B000, length = 0x000FF8 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
// RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* Only on F28379D, F28377D, F28375D devices. Remove line on other devices. */
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
CANA_MSG_RAM : origin = 0x049000, length = 0x000800
CANB_MSG_RAM : origin = 0x04B000, length = 0x000800
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0
.text : >> RAMD0 | RAMLS_ALL, PAGE = 0 // .text: >> RAMD0 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4,
.cinit : > RAMM0, PAGE = 0
.switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
#if defined(__TI_EABI__)
.bss : > RAMLS5, PAGE = 1
.bss:output : > RAMLS3, PAGE = 0 // I am getting error from here
.init_array : > RAMM0, PAGE = 0
.const : > RAMLS5, PAGE = 1
.data : > RAMLS5, PAGE = 1
.sysmem : > RAMLS5, PAGE = 1
#else
.pinit : > RAMM0, PAGE = 0
.ebss : > RAMLS5, PAGE = 1
.econst : > RAMLS5, PAGE = 1
.esysmem : > RAMLS5, PAGE = 1
#endif
Filter_RegsFile : > RAMGS0, PAGE = 1
ramgs0 : > RAMGS0, PAGE = 1
ramgs1 : > RAMGS1, PAGE = 1
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} > RAMM0, PAGE = 0
#else
ramfuncs : > RAMM0 PAGE = 0
#endif
#endif
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
/* The following section definition are for SDFM examples */
Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
Difference_RegsFile : >RAMGS5, PAGE = 1, fill=0x3333
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
I couldn't find any sample FreeRTOS project for the F28379D. Therefore, I examined the sample projects for the F28388D, but I still couldn't succeed. Because these files are very independent of each other.
Based on some solutions I found on ti e2e forum site (forum link), it was suggested that I could solve this issue by merging the ramls sections. However, since the .ebss section uses ramls3, that line gives an error.

I also try to write RAMLS_ALL to where I get error (.bss:output). Then I get this warning:
warning #10247-D: creating output section ".freertosStaticStack" without a SECTIONS specification warning #10247-D: creating output section ".freertosHeap" without a SECTIONS specification
Where can I find a .cmd file that will allow me to run FreeRTOS using the F28379D? I would appreciate any help you can provide.