Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Tool/software:
the example code 'led_ex2_blinky_sysconfig_multi' debug failed, what can I do to run the debug, below is my operation step.
1.I import the example from 'C2000Ware_5_02_00_00', and then build all the project.

2.Click the 'Debug' button to run the code, and an error about cpu2 generated.



3.I try to run the debug from 'Target Configurations' . I can load the CPU1 code, but the CPU2 code still load failed.