Other Parts Discussed in Thread: C2000WARE
Tool/software:
Our project used to run fine. The project contains a few modules which are all logically correct, which is verified in some way. But one module, let me call it "Module1", seems to have caused some memory issue.
- If commenting out "Module1", the whole project runs fine.
- If including "Module1", when running the project, some variables become strange, such as "-Inf" "NaN". "-Inf" means "minus infinite" and "NaN" means "not a number"? Below is the screen capture of the "Expression tab":

These variables are defined in "cla_shared" because they are used by both CPU and CLA
I believe it is a memory issue because "Module1" is logically correct. I guess there are 2 possibilities:
- stack overflow happened, or
- dynamic memory allocation (heap) issue
I tried to increase stack and heap size but failed to resolve the problem. Below is the .cmd file; could you advise how to fix it?
==========
MEMORY
{
BEGIN : origin = 0x080000, length = 0x000002 // Update the codestart location as needed
BOOT_RSVD : origin = 0x000002, length = 0x000126 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000128, length = 0x0002D8
RAMM1 : origin = 0x000400, length = 0x000400
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
/* Quentin 20240307: Combining all the LS RAMs */
//RAMLS012 : origin = 0x008000, length = 0x001800
//RAMLS12 : origin = 0x008800, length = 0x001000
RAMLS3 : origin = 0x009800, length = 0x000800
// RAMLS4 : origin = 0x00A000, length = 0x000800
// RAMLS5 : origin = 0x00A800, length = 0x000800
// RAMLS6 : origin = 0x00B000, length = 0x000800
// RAMLS7 : origin = 0x00B800, length = 0x000800
/* Quentin 20240110: Combining all the LS RAMs */
RAMLS4567 : origin = 0x00A000, length = 0x002000
RAMLS8 : origin = 0x014000, length = 0x002000 // When configured as CLA program use the address 0x4000
RAMLS9 : origin = 0x016000, length = 0x002000 // When configured as CLA program use the address 0x6000
// RAMLS8_CLA : origin = 0x004000, length = 0x002000 // Use only if configured as CLA program memory
// RAMLS9_CLA : origin = 0x006000, length = 0x002000 // Use only if configured as CLA program memory
//RAMGS0 : origin = 0x00C000, length = 0x002000
//RAMGS1 : origin = 0x00E000, length = 0x002000
RAMGS01 : origin = 0x00C000, length = 0x004000
RAMGS2 : origin = 0x010000, length = 0x002000
RAMGS3 : origin = 0x012000, length = 0x002000
/* Flash Banks (128 sectors each) */
FLASH_BANK0 : origin = 0x080002, length = 0x1FFFE
FLASH_BANK1 : origin = 0x0A0000, length = 0x20000
FLASH_BANK2 : origin = 0x0C0000, length = 0x20000
FLASH_BANK3 : origin = 0x0E0000, length = 0x20000
FLASH_BANK4 : origin = 0x100000, length = 0x20000
CLATOCPURAM : origin = 0x001480, length = 0x000080
CPUTOCLARAM : origin = 0x001500, length = 0x000080
CLATODMARAM : origin = 0x001680, length = 0x000080
DMATOCLARAM : origin = 0x001700, length = 0x000080
RESET : origin = 0x3FFFC0, length = 0x000002
}
SECTIONS
{
codestart : > BEGIN
.text : >> FLASH_BANK0 | FLASH_BANK1, ALIGN(8)
.cinit : > FLASH_BANK0, ALIGN(8)
.switch : > FLASH_BANK0, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
//.stack : > RAMM1
// Quentin 20240307: change .stack from RAMM1 to RAMLS0 for more space
//.stack : > RAMLS0
// Quentin 20240424: change .stack from RAMLS0 to RAMGS0: 1. for more stack space 2. for RAMLS0 used for CLA
//.stack : > RAMGS0
.stack : > RAMGS01
#if defined(__TI_EABI__)
//.bss : > RAMLS5
.bss : > RAMLS4567
//.bss:output : > RAMLS3
// Quentin 20240323: replace line above with line below, to leave RAMLS3 for other usage
//.bss:output : > RAMLS12
// Quentin 20240323: since I am not sure about correct usage of RAMLS8 as CLA memory, replace line above with line below to change from using RAMLS12 to RAMLS8
//.bss:output : > RAMLS8
// Quentin 20240525 : I am afraid putting .sysmem & .data together at RAMLS8 might cause problem, so replace RAMLS8 with RAMGS2
.bss:output : > RAMGS2
.init_array : > FLASH_BANK0, ALIGN(8)
.const : > FLASH_BANK0, ALIGN(8)
//.data : > RAMLS5 | RAMLS6
//.data : > RAMGS0
// Quentin 20240307: to prevent stack overflow to GSRAM, replace line(RAMGS0) above with line below(RAMLS12):
//.data : > RAMLS12
// Quentin 20240323: since I am not sure about correct usage of RAMLS8 as CLA memory, replace line above with line below to change from using RAMLS12 to RAMLS8
//.data : > RAMLS8
.data : > RAMLS9
//.sysmem : > RAMLS4
//.sysmem : > RAMGS0
// Quentin 20240307: to prevent stack overflow to GSRAM, replace line(RAMGS0) above with line below(RAMLS12):
//.sysmem : > RAMLS12
// Quentin 20240323: since I am not sure about correct usage of RAMLS8 as CLA memory, replace line above with line below to change from using RAMLS12 to RAMLS8
//.sysmem : > RAMLS8
// Quentin 20240525 : I am afraid putting .sysmem & .data together at RAMLS8 might cause problem, so replace RAMLS8 with RAMGS3
.sysmem : > RAMGS3
#else
.pinit : > FLASH_BANK0, ALIGN(8)
//.ebss : >> RAMLS5 | RAMLS6
.ebss : >> RAMLS4567
.econst : > FLASH_BANK0, ALIGN(8)
//.esysmem : > RAMLS5
.esysmem : > RAMLS4567
#endif
//ramgs0 : > RAMGS0
//ramgs1 : > RAMGS1
ramgs2 : > RAMGS2
#if defined(__TI_EABI__)
.TI.ramfunc : {} LOAD = FLASH_BANK0,
//RUN = RAMLS0,
RUN = RAMLS4567,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
#else
.TI.ramfunc : {} LOAD = FLASH_BANK0,
//RUN = RAMLS0,
RUN = RAMLS4567,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
ALIGN(8)
#endif
/* CLA specific sections */
#if defined(__TI_EABI__)
/* CLA specific sections */
Cla1Prog : LOAD = FLASH_BANK0,
RUN = RAMLS0,
LOAD_START(Cla1ProgLoadStart),
RUN_START(Cla1ProgRunStart),
LOAD_SIZE(Cla1ProgLoadSize),
ALIGN(4)
#else
/* CLA specific sections */
Cla1Prog : LOAD = FLASH_BANK0,
RUN = RAMLS0,
LOAD_START(_Cla1ProgLoadStart),
RUN_START(_Cla1ProgRunStart),
LOAD_SIZE(_Cla1ProgLoadSize),
ALIGN(4)
#endif
// below is from F28P55 cla_ex4_pwm_control example project (20240419)
Cla1ToCpuMsgRAM : > CLATOCPURAM
CpuToCla1MsgRAM : > CPUTOCLARAM
.scratchpad : > RAMLS1
.bss_cla : > RAMLS1
Cla1DataRam : > RAMLS2
cla_shared : > RAMLS1
CLADataLS1 : > RAMLS1
#if defined(__TI_EABI__)
.const_cla : LOAD = FLASH_BANK0,
RUN = RAMLS1,
RUN_START(Cla1ConstRunStart),
LOAD_START(Cla1ConstLoadStart),
LOAD_SIZE(Cla1ConstLoadSize),
ALIGN(4)
#else
.const_cla : LOAD = FLASH_BANK0,
RUN = RAMLS1,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize),
ALIGN(4)
#endif
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
CLA shared memory