Hi,
I am using to Code Composer Studio. I am trying to migrate an existing project from v3. to v4.
I used the import project wizard.( import legacy ccsv3.3 project) Then, I tried to fix some problems by adding some files , folders ( properties > C/C++ Build > Include
options ) and libraries ( properties > C/C++ Build > File search path ). I think that i should find another library to add my new project.
I am getting the following errors.
undefined first referenced
symbol in file
--------- ----------------
_clarke_calc E:/01_ti/04_ti_wspaces/05_motor/2xPM_Motors/2803x_RAM/2xPM_Motors.obj
_ipark_calc E:/01_ti/04_ti_wspaces/05_motor/2xPM_Motors/2803x_RAM/2xPM_Motors.obj
_park_calc E:/01_ti/04_ti_wspaces/05_motor/2xPM_Motors/2803x_RAM/2xPM_Motors.obj
_phase_voltage_calc E:/01_ti/04_ti_wspaces/05_motor/2xPM_Motors/2803x_RAM/2xPM_Motors.obj
_pid_reg3_calc E:/01_ti/04_ti_wspaces/05_motor/2xPM_Motors/2803x_RAM/2xPM_Motors.obj
_rampgen_calc E:/01_ti/04_ti_wspaces/05_motor/2xPM_Motors/2803x_RAM/2xPM_Motors.obj
_rmp_cntl_calc E:/01_ti/04_ti_wspaces/05_motor/2xPM_Motors/2803x_RAM/2xPM_Motors.obj
_speed_est_calc E:/01_ti/04_ti_wspaces/05_motor/2xPM_Motors/2803x_RAM/2xPM_Motors.obj
_svgendq_calc E:/01_ti/04_ti_wspaces/05_motor/2xPM_Motors/2803x_RAM/2xPM_Motors.obj
error: unresolved symbols remain
error: errors encountered during linking; "../2803x_RAM/2xPM_Motors.out" not
built
Thanks ,