Part Number: C2000WARE
Tool/software:
I have attempted to use the port given in the 5.02.0.0 version of the C2000Ware and got in trouble with interrupt priorities and having the tasks properly preempt after released from interrupts. Also the kernel was locking up constantly in the vListInsert() function.
My program was using a 1KHz tick and constantly running serial and SPI interfaces,
Most of the problem start showing when the system was stressed and the frequency of the interrupts would increase.
Attached are the modifications I made to get the port to work reliably.
(The local tick counter is not required, but used in my code to generate the statistics timer)
It would be very helpful if more users verified the modifications and provided feedback or further improvements to the code.
//-------------------------------------------------------------------------------------------------
// Author: Ivan Zaitsev, ivan.zaitsev@gmail.com
//
// This file follows the FreeRTOS distribution license.
//
// FreeRTOS is free software; you can redistribute it and/or modify it under
// the terms of the GNU General Public License (version 2) as published by the
// Free Software Foundation >>>> AND MODIFIED BY <<<< the FreeRTOS exception.
//
// ***************************************************************************
// >>! NOTE: The modification to the GPL is included to allow you to !<<
// >>! distribute a combined work that includes FreeRTOS without being !<<
// >>! obliged to provide the source code for proprietary components !<<
// >>! outside of the FreeRTOS kernel. !<<
// ***************************************************************************
//
// FreeRTOS is distributed in the hope that it will be useful, but WITHOUT ANY
// WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS
// FOR A PARTICULAR PURPOSE. Full license text is available on the following
// link: http://www.freertos.org/a00114.html
//-------------------------------------------------------------------------------------------------
// Modified: Joao Carlos Chies, joao.chies@sparton.com
// * Adjust use of preemptive configurations
// * Define local 32bits variable to optimized priority handling. FreeRTOS defines as UBaseType_t
// which is 16 bits in our case
// * Define a local tick counter, to use in place of xTaskGetTickCount() function
//-------------------------------------------------------------------------------------------------
//-------------------------------------------------------------------------------------------------
// Scheduler includes.
//-------------------------------------------------------------------------------------------------
#include "FreeRTOS.h"
#include "task.h"
//-------------------------------------------------------------------------------------------------
// Implementation of functions defined in portable.h for the C28x port.
//-------------------------------------------------------------------------------------------------
// Constants required for hardware setup.
#define portINITIAL_CRITICAL_NESTING ( ( uint16_t ) 10 )
#define portFLAGS_INT_ENABLED ( ( StackType_t ) 0x08 )
#if defined(__TMS320C28XX_FPU64__)
# define AUX_REGISTERS_TO_SAVE 27 // XAR + FPU registers
# define XAR4_REGISTER_POSITION 6 // XAR4 position in AUX registers array
# define STF_REGISTER_POSITION 10 // STF position in AUX registers array
#elif defined(__TMS320C28XX_FPU32__)
# define AUX_REGISTERS_TO_SAVE 19 // XAR + FPU registers
# define XAR4_REGISTER_POSITION 6 // XAR4 position in AUX registers array
# define STF_REGISTER_POSITION 10 // STF position in AUX registers array
#else
# define AUX_REGISTERS_TO_SAVE 9 // XAR registers only
# define XAR4_REGISTER_POSITION 5 // XAR4 position in AUX registers array
#endif
/* Let the user override the pre-loading of the initial LR with the address of
prvTaskExitError() in case it messes up unwinding of the stack in the
debugger. */
#ifdef configTASK_RETURN_ADDRESS
#define portTASK_RETURN_ADDRESS configTASK_RETURN_ADDRESS
#else
#define portTASK_RETURN_ADDRESS prvTaskExitError
#endif
extern uint32_t getSTF( void );
/*
* Setup the timer to generate the tick interrupts. The implementation in this
* file is weak to allow application writers to change the timer used to
* generate the tick interrupt.
*/
void vPortSetupTimerInterrupt( void );
// Each task maintains a count of the critical section nesting depth. Each
// time a critical section is entered the count is incremented. Each time a
// critical section is exited the count is decremented - with interrupts only
// being re-enabled if the count is zero.
//
// ulCriticalNesting will get set to zero when the scheduler starts, but must
// not be initialised to zero as this will cause problems during the startup
// sequence.
// ulCriticalNesting should be 32 bit value to keep stack alignment unchanged.
volatile uint32_t ulCriticalNesting = portINITIAL_CRITICAL_NESTING;
volatile uint16_t bYield = 0;
volatile uint32_t uxReadyPrioritiesPort = 0;
volatile uint32_t ulTickCounterPort = 0;
//-------------------------------------------------------------------------------------------------
// Initialise the stack of a task to look exactly as if
// timer interrupt was executed.
//-------------------------------------------------------------------------------------------------
StackType_t *pxPortInitialiseStack( StackType_t *pxTopOfStack, TaskFunction_t pxCode, void *pvParameters )
{
uint16_t i;
uint16_t base = 0;
pxTopOfStack[base++] = 0x0080; // ST0. PSM = 0(No shift)
pxTopOfStack[base++] = 0x0000; // T
pxTopOfStack[base++] = 0x0000; // AL
pxTopOfStack[base++] = 0x0000; // AH
pxTopOfStack[base++] = 0xFFFF; // PL
pxTopOfStack[base++] = 0xFFFF; // PH
pxTopOfStack[base++] = 0xFFFF; // AR0
pxTopOfStack[base++] = 0xFFFF; // AR1
pxTopOfStack[base++] = 0x8A08; // ST1
pxTopOfStack[base++] = 0x0000; // DP
pxTopOfStack[base++] = 0x0000; // IER
pxTopOfStack[base++] = 0x0000; // DBGSTAT
pxTopOfStack[base++] = ((uint32_t)pxCode) & 0xFFFFU; // PCL
pxTopOfStack[base++] = ((uint32_t)pxCode >> 16) & 0x00FFU; // PCH
pxTopOfStack[base++] = 0xAAAA; // Alignment
pxTopOfStack[base++] = 0xBBBB; // Alignment
// Fill the rest of the registers with dummy values.
for(i = 0; i < (2 * AUX_REGISTERS_TO_SAVE); i++)
{
uint16_t low = 0x0000;
uint16_t high = 0x0000;
if(i == (2 * XAR4_REGISTER_POSITION))
{
low = ((uint32_t)pvParameters) & 0xFFFFU;
high = ((uint32_t)pvParameters >> 16) & 0xFFFFU;
}
#if defined(__TMS320C28XX_FPU32__) || defined(__TMS320C28XX_FPU64__)
if(i == (2 * STF_REGISTER_POSITION))
{
uint32_t stf = getSTF();
low = stf & 0xFFFFU;
high = (stf >> 16) & 0xFFFFU;
}
#endif
pxTopOfStack[base + i] = low;
i++;
pxTopOfStack[base + i] = high;
}
base += i;
// Reserve place for ST1 which will be used in context switch
// to set correct SPA bit ASAP.
pxTopOfStack[base++] = 0x8A18; // ST1 with SPA bit set
pxTopOfStack[base++] = 0x0000; // DP
pxTopOfStack[base++] = 0x0000; // placeholder for 32 bit ulCriticalNesting
pxTopOfStack[base++] = 0x0000;
// Return a pointer to the top of the stack we have generated so this can
// be stored in the task control block for the task.
return pxTopOfStack + base;
}
//-------------------------------------------------------------------------------------------------
void vPortEndScheduler( void )
{
// It is unlikely that the TMS320 port will get stopped.
// If required simply disable the tick interrupt here.
}
//-------------------------------------------------------------------------------------------------
// See header file for description.
//-------------------------------------------------------------------------------------------------
BaseType_t xPortStartScheduler(void)
{
vPortSetupTimerInterrupt();
ulCriticalNesting = 0;
portENABLE_INTERRUPTS();
portRESTORE_FIRST_CONTEXT();
// Should not get here!
return pdFAIL;
}
//-------------------------------------------------------------------------------------------------
void vPortEnterCritical( void )
{
portDISABLE_INTERRUPTS();
ulCriticalNesting++;
}
//-------------------------------------------------------------------------------------------------
void vPortExitCritical( void )
{
ulCriticalNesting--;
if (ulCriticalNesting == 0)
{
portENABLE_INTERRUPTS();
}
}
//-------------------------------------------------------------------------------------------------
void vApplicationTickHook (void)
{
ulTickCounterPort++;
}
/*
* Setup the CPU timer 2 to generate the tick interrupts at the required
* frequency.
*/
#pragma WEAK( vPortSetupTimerInterrupt )
void vPortSetupTimerInterrupt( void )
{
//
// Initialize timer period:
//
CPUTimer_setPeriod(CPUTIMER2_BASE, configCPU_CLOCK_HZ / configTICK_RATE_HZ);
//
// Set pre-scale counter to divide by 1 (SYSCLKOUT):
//
CPUTimer_setPreScaler(CPUTIMER2_BASE, 0);
//
// Initializes timer control register. The timer is stopped, reloaded,
// free run disabled, and interrupt enabled.
// Additionally, the free and soft bits are set
//
CPUTimer_stopTimer(CPUTIMER2_BASE);
CPUTimer_reloadTimerCounter(CPUTIMER2_BASE);
CPUTimer_setEmulationMode(CPUTIMER2_BASE, CPUTIMER_EMULATIONMODE_STOPAFTERNEXTDECREMENT);
//
// Enable interrupt and start timer
//
CPUTimer_enableInterrupt(CPUTIMER2_BASE);
Interrupt_register(INT_TIMER2, &portTICK_ISR);
Interrupt_enable(INT_TIMER2);
CPUTimer_startTimer(CPUTIMER2_BASE);
}